Skip to main content
Visitor II
January 18, 2024
Question

LSM6DSL Self Test Thresholds

  • January 18, 2024
  • 1 reply
  • 1001 views

I have performed the self-test on LSM6DSL and observed that it was noted the thresholds mentioned in the datasheet

RamanaKumar_0-1705576951766.png

 

I want to know how these values of  90mg > xxx < 170mg  & 150 dps> xxx <700dps measured?

Why does the acceleration and gyro change when put in self test mode?

 

 

 

This topic has been closed for replies.

1 reply

Federica Bossi
Technical Moderator
January 19, 2024

Hi @RamanaKumar ,

Welcome to ST Community!

As described in Section 10 of the Application Note, the embedded self-test functions allows checking the device functionality without moving it. When the accelerometer self-test is enabled, an actuation force is applied to the sensor, simulating a definite input acceleration. In this case, the sensor outputs exhibit a change in their DC levels which are related to the selected full scale through the sensitivity value. The gyroscope self-test allows testing the mechanical and electrical parts of the gyroscope sensor: when it is activated, an actuation force is applied to the sensor, emulating a definite Coriolis force and the seismic mass is moved by means of this electrostatic test-force. In this case, the sensor output exhibits an output change.

The min-max values reported in the DS come from several tests done in production, there is piece to piece variability: on one part you will be able to measure 100mg as on another you will be able to see 1000mg.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.