Skip to main content
RNJ
Associate
March 15, 2023
Question

LSM6DSL - Temperature Accuracy

  • March 15, 2023
  • 1 reply
  • 949 views

We have several units of LSM6DSL in the field and I was looking that this part has an embedded temperature sensor. I would like to understand better the accuracy of this sensor. The datasheet is not clear, showing only this information.

0693W00000aJ3JmQAK.png 

Can I assume the operational range of this sensor is the same as the device (Top = -40~85ºC)?

The datasheet says OFFSET -15/+15 ºC. Is this the accuracy of this sensor? 

 Since is 16bits for ADC resolution, the minimal step will be 1/256 ºC. And the range will read 25ºC +/- 127ºC?

The AN5040 shows a table of example values

 0693W00000aJ3L9QAK.png 

Considering these values looks like each degree are part of the 8bit register, making 1bit/ºC and with integer values. Can anyone help me understand that?

    This topic has been closed for replies.

    1 reply

    Federica Bossi
    Technical Moderator
    April 5, 2023

    Hi @RNJ​ ,

    Welcome to ST Community!

    About your first question: yes, the operational range is -40-85°C.

    The datasheet says OFFSET -15/+15 ºC. Is this the accuracy of this sensor? No, this is the max an min offset meaning that if the room temperature is 25 degree the sensor can show 25+15 °C. Since this is an offset, it can removed by performing a calibration.

    In this case, if you are compensating the offset, considering that the LSB value is 1/256°, you could have an accuracy of about +-1.5°C across the +-1°C interval.

    Hope this helps.

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.