Associate
January 30, 2024
Question
LSM6DSM - Inquiry regarding 12-sec periodic noise
- January 30, 2024
- 1 reply
- 1655 views
I have been experiencing a peculiar issue with the LSM6DSM sensor, where noise occurs at a 12-second interval. This phenomenon is consistent across multiple units and locations. Notably, the noise seems to affect only the Z-axis.
Settings: with the ACC in operation and GYR disabled.
ODR 52Hz, +/-8G, the filter set to the state closest to RAW,
and a FIFO setup with a 3840-byte threshold. The data is not decimated in the FIFO.
It appears that the 3840-byte FIFO setting and the 52Hz ODR result in approximately a 12-second cycle. I am curious to understand the root cause of this issue and would appreciate any insights or recommendations for mitigating it.