Skip to main content
Associate II
April 28, 2025
Question

LSM6DSO32XTR Mode 2 (SensorHub) Setup with 2 Accelerometers, 2 Gyros, & Magnetometer

  • April 28, 2025
  • 0 replies
  • 289 views

Hi ST Community,

I’m trying to use the LSM6DSO32XTR in Mode 2 (SensorHub) to stream data from two accelerometers, two gyroscopes, and a magnetometer into the 9-kbyte Smart FIFO for motion tracking over 10–30 minutes, aiming for low MCU interrupts and power usage.

What I’ve Tried:

I’ve set up one LSM6DSO32XTR as the master (using its internal accelerometer and gyroscope) and planned to connect a second accelerometer (e.g., LIS2DH12), a second gyroscope (e.g., L3GD20H), and a magnetometer (e.g., LIS3MDL) on the secondary I²C bus (SCx/SDx).

I’m using Zephyr RTOS, referring to the datasheet (Section 7.2, 5.4), but learned I can’t connect another LSM6DSO32XTR as a slave on the secondary bus.

Questions:

1. Has anyone done a similar Mode 2 setup with these sensors? How did you handle I²C addressing?
2. Any pitfalls in the Mode 2 config to ensure FIFO streaming works?
3. Tips for power optimisation and avoiding data loss over long periods?
4. Any alternative methods for this multi-sensor setup?

I’d appreciate any insights or different approaches!