LSM6DSOX: configure MLC / UNICO to generate INT1 on only ONE specific gesture?
Hello ST community,
I am working with LSM6DSOX and using the Machine Learning Core (MLC) configured through UNICO GUI. My goal is to use the sensor as a low-power wake-up source for my system.
System overview:
MCU: nRF52840 (goes to deep sleep / system OFF)
Sensor: LSM6DSOX
Interface: I²C
Interrupt: INT1 used as hardware wake-up source
MCU is sleeping, so no software filtering is possible before wake-up
What I want to achieve
I want the MCU to wake up ONLY when one specific gesture occurs (for example a “wave” gesture).
INT1 should assert only for this one gesture
INT1 should NOT trigger for:
static state
random shake
other trained gestures
noise or motion not matching the target gesture
What I have already done
I successfully trained multiple gestures in UNICO GUI using MLC.
I can export and load the UCF correctly.
INT1 triggers when any gesture is detected.
I can read MLC status (Get_MLC_Status) after MCU wakes, but this does not help because:
The MCU must already be awake to do software filtering.
I need hardware-level filtering, since INT1 is the wake source.
Problems / limitations
Training only one gesture
Training with a single gesture often produces false positives.
In practice, accuracy improves when training with two or more gestures, but then:
INT1 triggers for all detected classes.
Interrupt behavior
INT1 appears to trigger on any MLC state change, not on a specific class.
I want INT1 to be asserted only for one Meta Classifier output (e.g., class 0).
UNICO configuration uncertainty
It is unclear how to:
Properly define “everything else” as negative class
Tune features / windows to avoid false wakeups
Map only one MLC class to INT1 at hardware level
My questions
Training question (UNICO / MLC)
What is the recommended way to train one wake-up gesture while ignoring all other motions?
Is it better to:
Train one gesture + “no motion”?
Train multiple gestures but only use one as wake-up?
Which UNICO features are recommended to minimize false positives for wake-up use cases?
Interrupt routing question
Is it possible to configure LSM6DSOX so that:
INT1 is asserted only for one specific MLC class (Meta Classifier index)?
Other classes do not toggle INT1 at all?
If yes:
Which register(s) should be used?
Should MLC_INT1 be programmed manually?
Is this configurable directly from UNICO with offline mode?
Best-practice question
What is the recommended ST approach for using LSM6DSOX MLC as a gesture-based wake-up source when the MCU is fully asleep?