Skip to main content
Associate
December 21, 2025
Solved

Lsm6dsv 9c boot loop after int

  • December 21, 2025
  • 2 replies
  • 291 views

1000002259.jpg

Hi i have a custom lsm6dsv  module  that is getting  a strange result  after 6a 9c then cycles through  int of the imu 9c seem to make it restart its process  and loop it for a for until 6a is back and 9c comes back and does the exact  same process   and unsure  what i should look at next [ i am new to logic  analyzing oscilloscope   scopes signals  seem fine  i feel like im missing  something  badly 

 

Parts 100nf caps 

5.1k resistor  tired  10k but I thought  lower  them could solve it? Before  I do anything  dumb I need input on what could cause this i can also provide logic files from pulse veiw 

Thanks

 

 

 

Best answer by Federica Bossi

Hi @Cutzo_500 ,

The repeated 6A and 9C bytes with NACKs suggest I²C communication issues. Possible causes include incorrect register reads, timing problems, or bus noise. Check pull-up resistor values (2.2kΩ–10kΩ), ensure clean SDA/SCL signals on the scope, verify correct I²C address and read sequences, and confirm proper start/stop conditions. Slowing down the I²C clock and reviewing your code and logic analyzer captures can help identify the problem.

2 replies

Federica Bossi
Federica BossiBest answer
Technical Moderator
December 24, 2025

Hi @Cutzo_500 ,

The repeated 6A and 9C bytes with NACKs suggest I²C communication issues. Possible causes include incorrect register reads, timing problems, or bus noise. Check pull-up resistor values (2.2kΩ–10kΩ), ensure clean SDA/SCL signals on the scope, verify correct I²C address and read sequences, and confirm proper start/stop conditions. Slowing down the I²C clock and reviewing your code and logic analyzer captures can help identify the problem.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Cutzo_500Author
Associate
December 24, 2025

Thank you for the feedback  i did confirm  that shortly  after a oscilloscope  dig and found my bi solder to be unreliable  for this lga packages  and give a grainy  result  visual and confirmed after it was left for a bit a  when slient  logic and scope wise 

Do you have any recommendations  for sac or leaded  solder for these footprint reliablty  sac perrfered I dont want to risk another  project  from a bad choice  of solder brand