Skip to main content
Visitor II
November 25, 2024
Question

MotionFX shows bias on the axis that is under gravity influence

  • November 25, 2024
  • 1 reply
  • 3407 views

Hi, 

I am using MotionFX with BlueCoin, for a solution that can detect vertical movement within 2 meter range with high precision.  

I took the ALLMEMS2 example when I logged linear acceleration and gravity, it showed some unprecise values like

linear acceleration around 0.2 when the device wasn't moving. When I increased the full scale factor for ACC to 16.0f and Gyro to 2000dps, the linear acceleration value improved to the range of 0.05-0.1, which is still not as expected. 

Gravity value is strangely too high and stable 9.99, shouldn't it be closer to 9.81 max in the stale state?

 

 

NFO:__main__:Linear Acc -> x: 0.0290, y: -0.0090, z: 0.0190
INFO:__main__:Gravity -> x: 0.0590, y: 0.0310, z: 9.9990
INFO:__main__:Linear Acc -> x: 0.0090, y: -0.0180, z: 0.0490
INFO:__main__:Gravity -> x: 0.0580, y: 0.0300, z: 9.9990
INFO:__main__:Linear Acc -> x: -0.0110, y: -0.0190, z: 0.0390
INFO:__main__:Gravity -> x: 0.0580, y: 0.0310, z: 9.9990
INFO:__main__:Linear Acc -> x: -0.0010, y: -0.0180, z: 0.0490
INFO:__main__:Gravity -> x: 0.0590, y: 0.0300, z: 9.9990
INFO:__main__:Linear Acc -> x: 0.0090, y: -0.0090, z: 0.0290
INFO:__main__:Gravity -> x: 0.0590, y: 0.0300, z: 9.9990
INFO:__main__:Linear Acc -> x: 0.0190, y: -0.0090, z: 0.0390
INFO:__main__:Gravity -> x: 0.0590, y: 0.0300, z: 9.9990
INFO:__main__:Linear Acc -> x: 0.0090, y: -0.0090, z: 0.0190
INFO:__main__:Gravity -> x: 0.0580, y: 0.0290, z: 9.9990
INFO:__main__:Linear Acc -> x: 0.0080, y: -0.0200, z: 0.0290

 

 

At first, I thought that I needed to calibrate ACC and Gyro, but their values are pretty good.

 

 

Accelerometer: {'x': 16, 'y': -4, 'z': -985}
Gyroscope: {'x': 1, 'y': 7, 'z': 4}
Magnetometer: {'x': -59, 'y': 252, 'z': 53}
------------------------------
Timestamp: 166960 ms
Accelerometer: {'x': 18, 'y': -3, 'z': -985}
Gyroscope: {'x': -4, 'y': 0, 'z': 3}
Magnetometer: {'x': -57, 'y': 252, 'z': 51}
------------------------------
Timestamp: 167008 ms
Accelerometer: {'x': 16, 'y': -4, 'z': -987}
Gyroscope: {'x': 0, 'y': 8, 'z': 3}
Magnetometer: {'x': -57, 'y': 257, 'z': 48}
------------------------------
Timestamp: 167056 ms
Accelerometer: {'x': 15, 'y': -3, 'z': -989}
Gyroscope: {'x': 0, 'y': 7, 'z': 3}
Magnetometer: {'x': -54, 'y': 260, 'z': 57}

 

 

So I suspect that something strange happening inside MotionFX library, which constantly shows a gravity value of 9.99 and introduces bias to vertical axes. 

 

Can I somehow improve bias for the vertical context?  

 

1 reply

Federica Bossi
Technical Moderator
December 6, 2024

Hi @vlad_kost ,

Some error is expected, in this case we are talking about 0.2 which is negligible.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.