Skip to main content
ALT.1
Associate
June 7, 2023
Question

MotionMC calibration process.

  • June 7, 2023
  • 0 replies
  • 970 views

Hello everyone. I make some project based on MotionMC and MotionEC libs. It's a magnetic compass which will use inside the cars. Within the MotionMC library, the end device functions properly if calibrated according to section 2.2.5 of the UM2192 manual ("figure eight" pattern). My issue is that the compass is firmly fixed inside the car, so it is not possible to calibrate it using the "figure-eight" method :beaming_face_with_smiling_eyes: Is there any alternative calibration method available for the MotionMC library that is suitable for use in a car? For example, rotating the compass in a circle within one plane or manually entering constants? Or is the MotionMC library not suitable for this task, and should I look for an alternative? Regards.

This topic has been closed for replies.