Skip to main content
JKing.3
Associate II
December 20, 2023
Question

MP23DB02MM Frequency Range

  • December 20, 2023
  • 2 replies
  • 1547 views

I interested in the higher frequency range of this device. The datasheet states clearly the LF cutoff at 35Hz, but there is no real discussion on the HF end apart from the characteristic graphs stopping at 10KHz. The device can be clocked up to 3.3MHz so it would seem that there is scope for higher frequencies. Is there any characteristics or design information for going above 10KHz and what are the tradeoffs? I see from some other posts that SNR is affected as the clock frequency increases.

Any guidance appreciated.

Thanks

Julian 

This topic has been closed for replies.

2 replies

Peter BENSCH
Technical Moderator
December 20, 2023

Well, the generic type of a microphone is typically intended either for speech or for high frequencies such as ultrasound. The typical range of speech is approximately between 200Hz and 2kHz, so the 10kHz mentioned in the data sheet already extends this limit quite well upwards. You can also process up to 20kHz with the microphone. At higher frequencies, the internal filter function becomes effective due to internal digitization.

If higher frequencies such as the ultrasound mentioned above are to be processed, a suitable MEMS microphone with an analog interface, i.e. without the digital interface, must be used, which then also requires analog processing, e.g. the IMP23ABSU.

Hope that helps?

Regards
/Peter

JKing.3
JKing.3Author
Associate II
December 20, 2023

Thank you for your reply Peter. I was hoping I might stretch the microphone to the frequencies we need, which is 25 & 33KHz, but looks like we'll have to go analogue.

Regards

Julian

Federica Bossi
Technical Moderator
December 20, 2023

Hi @JKing.3 ,

The maximum frequency you can acquire is 20kHz by design.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JKing.3
JKing.3Author
Associate II
December 20, 2023

Hi Freerica,

What happens above 20KHz, is there a predictable roll off or something less predictable.

Thanks

Julian

 

Federica Bossi
Technical Moderator
December 20, 2023

Hi @JKing.3 ,

There is a sensitivity rolloff that depends on the gasket in which the microphone is mounted (https://www.st.com/resource/en/application_note/an4427-gasket-design-for-optimal-acoustic-performance-in-mems-microphones-stmicroelectronics.pdf)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.