Skip to main content
BLegg
Visitor II
May 22, 2019
Question

OUTPUT FROM ACCELERATION SENSOR LSM303

  • May 22, 2019
  • 1 reply
  • 873 views

I am using a LSM303DLHC and setting it up with:

// CTRL_REG1_A (0x20) loaded with 0x27 = 00100111, 10hZ rate,normal power enable X,Y,Z on

Write_Register(ACC_I2C_ADDRESS,0x20,0x27);

// CTRL_REG4_A (0x23) loaded with 0x40 = 01000000, big endian, +/-2g

Write_Register(ACC_I2C_ADDRESS,0x23,0x40);

And reading the registers as follows:

ACC_Data[0] = Read_Register(ACC_I2C_ADDRESS,0x28);  // read out x MSB

ACC_Data[1] = Read_Register(ACC_I2C_ADDRESS,0x29);  // read out x LSB

But I am betting odd results like:

Ax:-16160  Ay:-16352  Az:192

When the sensor is 'flat' ie X and Y horizontal and Z vertical.

The output range seems to be about zero to -32,000? Is this correct?

Regards Bill Legge

    This topic has been closed for replies.

    1 reply

    Associate
    July 5, 2023

    The range of the entire 2 bytes is -32,727. However, this gets further divided by 2 because the range of the readings is 2G. 16,000+/- "counts" means that you are reading 1G. This is completely normal.

    I agree that is seems like your output should be 32,727 for 90 degrees (gravity), but this is normal behavior. 

    Federica Bossi
    Technical Moderator
    July 5, 2023

    Hi @BLegg ,

    @wb346 is right, it is absolutely normal.

    In addition I suggest you to enable also Block Data Update (bit '7' reg CTRL_REG4_A (23h)).

    If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.