Skip to main content
Associate II
November 14, 2022
Solved

Output type of INT1 pin on ISM330DHCX

  • November 14, 2022
  • 2 replies
  • 1667 views

Hello,

I cannot find any detail about the output type of INT1 pin in the ISM330DHCX datasheet.

From what I read about the registers configuration about this pin, I thought that would be a push-pull output, but if I configure an external 10K pull-up to 3.3V I see that the signal is fixed to 1.2V

I already found the note about the initialization procedure that depict not to set any pull-up (so I'm removing that), but this behavior is not explained by a simply output pin.

Is maybe this also a bootstrap input for internal use?

For the use with the linux driver st_lsm6dsx (that has this component's compatible) should I set a pull-down or leave the control only to the ISM330DHCX?

Best regards,

Rosario

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    The function of pin INT1 is described in the data sheet:

    INT1_CTRL (section 9.9) manages the signals that are output by ORing

    CTRL3_C (section 9.14) describes at which level INT1 is active (H_LACTIVE) and whether INT1 works as push-pull or open drain.

    Does it answer your question?

    Regards

    /Peter

    2 replies

    Peter BENSCH
    Peter BENSCHBest answer
    Technical Moderator
    November 14, 2022

    The function of pin INT1 is described in the data sheet:

    INT1_CTRL (section 9.9) manages the signals that are output by ORing

    CTRL3_C (section 9.14) describes at which level INT1 is active (H_LACTIVE) and whether INT1 works as push-pull or open drain.

    Does it answer your question?

    Regards

    /Peter

    RBors.1Author
    Associate II
    November 14, 2022

    Hello Peter,

    yes, these are the information that I needed.

    Best regards,

    Rosario

    Peter BENSCH
    Technical Moderator
    November 14, 2022

    Great!

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Regards

    /Peter