Skip to main content
Visitor II
March 21, 2025
Solved

Query about MDRDY Signal Configuration in LSM6DSO16IS MODE2

  • March 21, 2025
  • 1 reply
  • 418 views

I am working with the LSM6DSO16IS in MODE2 configuration with ISPU enabled. I have some questions regarding the MDRDY (Master Data Ready) signal:

1. How is the MDRDY signal handled in MODE2 when using the master I2C interface with external sensors?

2. Is there any specific configuration needed in DRDY_PULSED_REG (0x0B) for proper MDRDY operation in MODE2?

3. Can you provide information about the timing relationship between MDRDY and the external sensor's data ready signal in MODE2?

4. Are there any application notes or reference designs specifically addressing MDRDY usage in MODE2?

Current configuration:

- Like JP4 from X-NUCLEO-IKS4A1 SCH, the INT2 of LSM6DSO16IS is connected to the interrupt output of an external sensor

- LSM6DSO16IS in MODE2
- ISPU enabled
- External sensor connected via master I2C
- Using X-CUBE-ISPU framework

Best answer by Federica Bossi

Hi @seanfan ,

1. MDRDY is a data ready signal from the external sensor brought to INT2. If properly configured (see step 2), the signal on INT2 becomes the trigger to perform the read/write operations configured on the sensor hub. This is explained in section 6.1 of the application note.
2. DRDY_PULSED_REG is used to configure the mode (pulsed/latched) of the interrupt generated by the sensor; it has nothing to do with the external sensor or mode 2. To use INT2 as an external trigger for the sensor hub, the START_CONFIG bit in the MASTER_CONFIG register must be set to 1. I recommend reading the bit description and note in section 6.2.1 of the application note.
3. MDRDY is the data ready signal from the external sensor carried on pin INT2.
4. The information available is in section 6 of the application note on using mode 2/sensor hub

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
March 27, 2025

Hi @seanfan ,

1. MDRDY is a data ready signal from the external sensor brought to INT2. If properly configured (see step 2), the signal on INT2 becomes the trigger to perform the read/write operations configured on the sensor hub. This is explained in section 6.1 of the application note.
2. DRDY_PULSED_REG is used to configure the mode (pulsed/latched) of the interrupt generated by the sensor; it has nothing to do with the external sensor or mode 2. To use INT2 as an external trigger for the sensor hub, the START_CONFIG bit in the MASTER_CONFIG register must be set to 1. I recommend reading the bit description and note in section 6.2.1 of the application note.
3. MDRDY is the data ready signal from the external sensor carried on pin INT2.
4. The information available is in section 6 of the application note on using mode 2/sensor hub

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.