Skip to main content
Eleon BORLINI
ST Employee
January 31, 2022
Solved

*** QVAR sensing - A new concept of sensor in ST portfolio ***

  • January 31, 2022
  • 4 replies
  • 7994 views

A new sensor has been recently launched on st.com, embedded in existing pressure and iNemo sensors: an electrostatic sensor that can be used for human presence and motion detection, touch detection, and user interface (UI) applications

Qvar stands for electric charge (= Q) variation (= var). It is an electrical potential sensing channel able to measure the quasi-electrostatic potential changes. ILPS22QS and LSM6DSV16X sensors allow to connect an analog input and convert it to a digital signal for embedded processing. In addition, the embedded Qvar channel can be enabled for sensing in applications such as water leakage detection, tap, double tap, long press, and L/R - R/L swipe.

0693W00000JNuBNQA1.png

Best answer by Eleon BORLINI

Additional information can be found on:

Share your comment here below, if you want!

4 replies

Eleon BORLINI
Eleon BORLINIAuthorBest answer
ST Employee
January 31, 2022

Additional information can be found on:

Share your comment here below, if you want!

kSun.1
Associate
April 16, 2022

I am very interested in this Qvar. What i understand is this Qvar depends on the electrode discharge and the Qvar wants to take advantage of ESD, is it correct? Also Does the Electrode pad size affect sensing ability? Do we always need ESD Diode to protect the Chip ?

Eleon BORLINI
ST Employee
April 20, 2022

Hi @kSun.1​ ,

The ESD diode are mandatory to protect the QVAR lines from electrostatic and electromagnetic discharges that goes beyond the absolute maximum rating that the QVAR can withstand. The dimension of the electrode pad affects the "wireless" electric field sensing, while it is pretty negligible for the QVAR contact sensing.

-Eleon

Associate II
September 14, 2024

I have a X-NUCLEO-IKS4A1 board connected to a STM32F401RE nucleo board and I also have the detachable add-on board STEVALMKE001A, which hosts the Qvar swipe electrodes. When I flash DataLogExtended firmware in Nucleo board and open Unicleo-GUI or MEMS Studio I enable Qvar buttom but the value I see is constant and, even if I touch in rapid succession one button and the other, the value never changed (is -420.103 mV when i select the LSM6DSV16X sensor and -860.366 mV when I select LIS2DUXS12 sensor). What can be the problem?

Visitor II
September 19, 2025

Hi @marti3110 -- Happy 1 year to your issue! I found that while using my X-NUCLEO-IQS4A1A, I had to move jumpers on J4 and J5 from QVAR GND to QVAR ENABLED. Now MEMS Studio shows appropriate data from the QVAR sensors. Was there something comparable on the IKS4A1 / did it work?