Skip to main content
Nicolas Goy
Associate II
February 15, 2023
Question

Selecting a motion sensor

  • February 15, 2023
  • 1 reply
  • 758 views

Hi,

I am looking for a motion sensor with I2C that can work in the following way:

  1. Wake up from low power
  2. Start monitoring acceleration and rotation
  3. Stop monitoring (about 500ms later)
  4. Query most significant motion while monitoring
  5. Go back to sleep

Basically the MCU will wake up the sensor, reset it's memory and then do other things (like reading other sensors..) and when done, about 500ms later, ask the sensor what was the most significant motion change during this time.

I read a few datasheet, and found some sensors with a FIFO, like the LSM6DSO, but it would require reading all data and do the aggregation on the MCU.

I would really love a chip that can provide a single "summary" of the motion.

It is important to have small sleep power consumption, but it seems they are all in the uA range, so it is good enough.

This topic has been closed for replies.

1 reply

Nicolas Goy
Associate II
February 21, 2023

I found the ISM330IS which would allow me to write a firmware, I guess that would work, but I am wondering if a simpler solution exists.