SensorTile
- August 4, 2023
- 2 replies
- 6360 views
At the moment I am making an application for 3D sound detection, in which I am making use of the STEVAL-STWINKT1B and the STEVAL-STWINMAV1 microphone array (which I haven't used yet). I am just starting, and I can not understand the operation of the SensorTile, previously I was using the SensorTile.box and it was easier to handle APP ST BLE SENSOR, in which I could easily extract the data, however, in the SensorTile it is getting complicated, I guess it is because of the FW used that I can not see the APP as in "cap2" and rather I see it as in "cap1".
Finally, speaking of the microphone array, I would like to ask how to connect it to the device? physically I have already connected it (in the CN4) but I understand that this is not enough to make use of it (besides I am not very clear how to receive the data that it gives me).
Sorry for so many doubts.