Skip to main content
Associate
May 6, 2025
Solved

SensorTile.Box PRO and STEVAL-MKI168V1

  • May 6, 2025
  • 2 replies
  • 471 views

Hi, 

I have an evaluation board STEVAL-MKI168V1 with the sensor IIS2DH. I was hoping to plug it into the DIL24 connector of the SensorTile.Box PRO and be able to see the sensor's output using the MEMS Studio. This does not seem to be the case. Can somebody provide me some guidance on how to access the sensor data using the SensorTile Box? Currently I am running the firmware FP-SNS-Datalog2 v 3.0.0. 

I saw that the Git repository https://github.com/STMicroelectronics/fp-sns-datalog2 includes drivers for the the sensor IIS2DH, so it looks like it should be possible to access the sensor somehow. 

 

Thanks,

Michal

 

Best answer by Federica Bossi

Hi @msv ,

Tto use the dil24 for sensortile.box pro it is necessary to program the board with the extended datalog firmware directly from the memsstudio software.
Support for the IIs2dh sensor will be available in the coming week with version 2.1.0 of the datalog firmware.

2 replies

Federica Bossi
Federica BossiBest answer
Technical Moderator
May 7, 2025

Hi @msv ,

Tto use the dil24 for sensortile.box pro it is necessary to program the board with the extended datalog firmware directly from the memsstudio software.
Support for the IIs2dh sensor will be available in the coming week with version 2.1.0 of the datalog firmware.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
msvAuthor
Associate
May 23, 2025

Could you please provide me with a link to the firmware if that is released already?

msvAuthor
Associate
May 15, 2025

Hi Federica, 

thanks for your answer. Isn't the current version the "FP-SNS_DATALOG2_Datalog2 v3.0.0"? So maybe you meant 3.1.0?

Thanks