Skip to main content
Associate
December 18, 2023
Solved

SensorTile.box PRO Expert Mode logging both Gyroscope and Microphone

  • December 18, 2023
  • 1 reply
  • 1154 views

Hi!

I am using the SensorTile.box PRO in Expert Mode and try to log both Gyroscope and Microphone on the SD Card.

When I try to upload the App I receive this error message: "There was a timeout error loading the App on the board".

If I make an App to log only Gyro or only Microphone the App is uploaded and everything runs ok (in the first case a .csv is generated while in the second a .wav is generated).

Thank you!

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @Gerva ,

Welcome to ST Community!

can you check the version of the app you are using?

it should not be possible to upload a flow with both microphone and gyroscope log to sd, using the default fw (the latest version should tell you about this problem).

 

there are several ways to enable gyro and mic log, for the easiest one you need to use another fw: the DATALOG2, that is the most powerful one for logging on sd card.

you can download it by downloading the new ST BLE Sensor app from the store, connecting to the board and go in the board configuration tab, select firmware download and search for the DATALOG2. (you can also download the package from st.com and upload the binary file in DFU mode, following the instruction on the Application Note of the board)

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
December 20, 2023

Hi @Gerva ,

Welcome to ST Community!

can you check the version of the app you are using?

it should not be possible to upload a flow with both microphone and gyroscope log to sd, using the default fw (the latest version should tell you about this problem).

 

there are several ways to enable gyro and mic log, for the easiest one you need to use another fw: the DATALOG2, that is the most powerful one for logging on sd card.

you can download it by downloading the new ST BLE Sensor app from the store, connecting to the board and go in the board configuration tab, select firmware download and search for the DATALOG2. (you can also download the package from st.com and upload the binary file in DFU mode, following the instruction on the Application Note of the board)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.