Skip to main content
Visitor II
July 1, 2025
Question

Serial (COM) Port for reading IMU data from STEVAL-MKI109D

  • July 1, 2025
  • 1 reply
  • 346 views

Dear all,
I would be interested to use a MKI109D dev board (with USB C connector) to stream data from a MKI178V2 board fitted with a SM6DSL IMU sensor to a preferably a python or cpp based script using something like a pyserial library. I have tested the board and the IMU with the MEMS Studio software and flashed it with the correct firmware , and therefore can see the IMU output as intended. However when trying to connect  to the dev board using pyserial, after opening the COM port , and transmitting the *dev command, I receive an error that the device is not supported. I would appreciate some help on some direction as to what the problem here might be and if possible a minimal set of python (or cpp) command to read out the IMU data. 
Many thanks in adveance.  

1 reply

Billy OWEN
ST Employee
July 2, 2025

Hi @SaeidD 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy