Skip to main content
Associate
May 6, 2025
Solved

STEVAL-IDP005V1-GUI does not connect

  • May 6, 2025
  • 1 reply
  • 718 views

Hi.

i am having a STEVAL-IDP005V1, STEVAL-UKI001V1, 10-pin-IDP005V1 Cable, M12female connector.

i am referring this document ( https://www.st.com/resource/en/product_presentation/steval-bfa001v1b_quick_start_guide.pdf ) 

i am not able to connect the board to my PC.  please anyone suggest me to do the analysis of accelerometer

is that any clear document? 

Thank you  

Best answer by AmrithHN

Are you using the swd connector? 

Make sure you are powering the device 18V or higher as per the requirement

The swd connector at the steval , how did you connect to it ? whats the orientation?

1 reply

AmrithHNBest answer
Associate III
May 6, 2025

Are you using the swd connector? 

Make sure you are powering the device 18V or higher as per the requirement

The swd connector at the steval , how did you connect to it ? whats the orientation?

Associate
May 6, 2025

Yes, i am using the SWD Connector. 
Yes, i applied the input voltage is 18.5 V. (brown Positive and blue negative)
Please refer the Picture.

IMG_20250506_122201.jpgIMG_20250506_122232_1.jpgIMG_20250506_122250.jpgIMG_20250506_122255.jpg

 

Associate III
May 6, 2025

I don’t recall the exact orientation of the connector on the st board but you can try connecting the swd connector on stm32 in the reverse direction (I had similar issue and I figured out that the connector needs to be connected in reverse direction and then it worked)

 

Also the baud rate is mentioned in the manual make sure to set that