Skip to main content
Tvan .5
Visitor II
November 19, 2020
Question

STEVAL-IDP005V1-GUI does not connect

  • November 19, 2020
  • 2 replies
  • 970 views

Hi

I am trying to run the STEVAL-IDP005V1-GUI.

Current setup:

STEVAL-IDP005V1-GUI - > STEVAL-IDP004V1->STEVAL-IDP005V1:

I am unable to connect to the IDP004V1 dev kit from the GUI, the comms just gives an error suggesting to restart the GUI. I have tried re flashing the firmware with the 485 and USB binaries provided in en.stsw-io-link (https://www.st.com/content/st_com/en/products/embedded-software/evaluation-tool-software/stsw-io-link.html)

I have tried both 485 and USB connections but it does not work. Please advise on how to get the demo's up and running

Regards

    2 replies

    Eleon BORLINI
    ST Employee
    November 23, 2020

    Hi @Tvan .5​ ,

    if you are using the STEVAL-IDP005V1 in conjunction to the STEVAL-BFA001V1B master board, the issue could be related to the fact described here, that is the cable description is wrong the ground is on white, not on blue wire.

    If you are using the STEVAL-IDP005V1 in conjunction to the STEVAL-IDP004V1 master board, the issue could be the one reported on Github here, but I don't actually know if it has been solved...

    -Eleon

    Associate III
    March 12, 2025

    At least make corrections in the documentation thats available in the website , i connected it as per the documentation and does it mean the stm32 is fried ?

    Will it work if i change the connection?

    Associate
    May 6, 2025

    Hi.

    i am having a STEVAL-IDP005V1, STEVAL-UKI001V1, 10-pin-IDP005V1 Cable, M12female connector.

    i am referring this document ( https://www.st.com/resource/en/product_presentation/steval-bfa001v1b_quick_start_guide.pdf ) 

    i am not able to connect the board to my PC.  please anyone suggest me to do the analysis of accelerometer

    is that any clear document? 

    Thank you