Skip to main content
Associate
June 20, 2024
Question

STEVAL-MKBOXPRO firmware that is compatible with ISPU dil24

  • June 20, 2024
  • 1 reply
  • 1023 views

I'm trying to make a demo with the ispu chip ism330is and the STEVAL-MKBOXPRO the issue is I can't find a suitable firmware for the tilebox pro that is compatible with the ispu and allows me upload the compiled UCF program into the chip. Below is a screenshot of the current firmware I'm using FPSNS DATALOG 2 in which it shows the ispu as unknown and if I try to upload the UCF it's just gets stuck!

 

1 reply

Federica Bossi
Technical Moderator
June 28, 2024

Hi @benx1326 ,

Welcome to ST Community!

Unfortunately ISM330IS firmware for STEVAL-MKBOXPRO is not currently available. We are working on it and it will release in future.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.