Skip to main content
nicolas
Senior II
October 6, 2025
Question

STEVAL-STWINBX1 examples doesn't respect STM32U585 datasheet

  • October 6, 2025
  • 1 reply
  • 443 views

The datasheet of STM32U585 say that "For operation with voltage higher than Min (VDD, VDDA, VDDUSB, VDDIO2) +0.3 V, the internal pull-up and pull-down resistors must be disabled." (chap. 5.3.1).
The STEVAL-STWINBX1 use a VDDA of 2.75V and a VDD of 3.3V => Min (VDD, VDDA, VDDUSB, VDDIO2) +0.3 V = 3.05V < VDD = 3.3V.
But in the examples provided for STEVAL-STWINBX1, pull up and down are used with a VDD of 3.3V.
So which is correct, the datasheet or the examples ?

1 reply

Amel NASRI
Technical Moderator
October 9, 2025

Hi @nicolas ,

Reviewing the product datasheet, I think that you are referring to the following note:

AmelNASRI_0-1760026503246.png

This note is applicable for VIN (the voltage input that may be applied for device pins) and not to VDD:

AmelNASRI_1-1760026546342.png

Therefore, I believe that the STEVAL-STWINBX1 design aligns well with the operating conditions described in the datasheet and in AN5373Getting started with STM32U5 MCU hardware development.

Additionally, I received confirmation that the STEVAL-STWINBX1 has been used for a considerable time with various firmware and demos without any reported issues.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
nicolas
nicolasAuthor
Senior II
October 10, 2025

I'm using SDDataLogFileX with STEVAL-STWINBX1. In the code i saw that pull up are used for I2C2 (I2C2_MspInit). When measuring on the I2C2 pins, i saw a signal that go up to ~3.2V. So for my understanding it doesn't respect the datasheet because it's higher than 2.75V + 0.3V.

Amel NASRI
Technical Moderator
October 10, 2025

I assume that there is no external voltage input for the I2C pin, so it is normal that the voltage is aligned with VDD.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.