Skip to main content
Macneacail
Associate III
February 4, 2023
Question

The 109 hang picture from the code. This is on old NUCs, modern NUCs and DELL precision. It is completely random but annoying.

  • February 4, 2023
  • 4 replies
  • 1564 views

..

    This topic has been closed for replies.

    4 replies

    Federica Bossi
    Technical Moderator
    April 7, 2023

    Hi @Macneacail​ ,

    To configure the device you need to issue the following sequence of commands:

    *setdb210v2

    *zoff 

    Hope this helps.

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
    Macneacail
    Associate III
    April 7, 2023

    Theoretically yes, practically no. The device has a little green light in the middle of the array of 3 LED's. When you start these should be off, but if you are running and the program stops, for whatever reason, then the green light is left on, then you need to unplug the device from the NUC, because just rebooting the NUC does not turn off the device. I have 12 of these all over the world it is a common problem.

    They do not unlock and they do not answer to commands if green light lit. This is from reading the buffer.

    This is what our program looks like at the moment, it is supposed to be running at 1666 Hz.


    _legacyfs_online_stmicro_images_0693W00000bhj7LQAQ.pngit is not, I have asked your MEMS people these questions a few months ago, some things not answered. The lack of a real serial number is a pain to by the way.

    Macneacail
    Associate III
    April 7, 2023

    UNICO GUI needs to be fixed by the way.

    Federica Bossi
    Technical Moderator
    April 7, 2023

    Hi @Macneacail​ ,

    I'm sorry for that.

    Are using Unico-GUI or only the firmware for STEVAL-MKI109V3?

    Have you already look at the user manual UM2116?

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.