Skip to main content
WrenchInTheWorks
Associate II
July 10, 2025
Solved

Three qestions about MotionFX CM0+

  • July 10, 2025
  • 3 replies
  • 625 views

Hello wonderfull STM community,

Really enjoying the experience with MotionFX so far, really easy to implement and get working, well done ST! Even on a G0 in CM0+ mode its working well! I'm just woudring three things:

  1. What precaution(s), if any, should be taken when pausing and later resuming the RTOS task that runs MotionFX_CM0P_update()?
  2. What is the refrence point for the quatenion in 6x mode? (to be fair I have not worked much with quatenions before so that might be an uneducated question. They are quite complex after all! (pun intended)) 
  3. Is it normal for data_out.rotation_6x to be near 0 (e-16) during oppration in 6 axis mode? (other values, inlcuding inputs, are changing as expected)

 

WrenchInTheWorks_0-1752136756774.png

 

Note that mag is just uninitialized, the values are those of what was already in memory, I should fix that, through this is the first I've noticed it.

Thanks and happy coding! 

Best answer by Federica Bossi

Hi @Pantera_MXJ ,

I share also here the corrected code you posted on the other topic, so that if someone else in the future encounters the same issue can solve:

/**
 ******************************************************************************
 * File Name : app_mems.c
 * Description : This file provides code for the configuration
 * of the STMicroelectronics.X-CUBE-MEMS1.11.3.0 instances.
 ******************************************************************************
 * @attention
 *
 * JMX Fusion Terminal JUL 17 2025
 * 
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */

#ifdef __cplusplus
extern "C" {
#endif

/* Includes ------------------------------------------------------------------*/
#include "app_mems.h"
#include "main.h"
#include <stdio.h>
#include <string.h>

#define _USE_MATH_DEFINES
#include <math.h>

#include "iks02a1_motion_sensors.h"
#include "stm32u5xx_nucleo.h"
#include "motion_fx.h"
#include "iks02a1_mems_control_ex.h"

/* Private typedef -----------------------------------------------------------*/
typedef enum {
 APP_STATE_CALIBRATING,
 APP_STATE_RUNNING
} AppState_t;

/* Private define ------------------------------------------------------------*/
#define SAMPLING_FREQ_HZ 100
#define SAMPLING_PERIOD_MS (1000 / SAMPLING_FREQ_HZ)
#define STATE_SIZE (2450)
#define PRINT_FREQUENCY_HZ 5
#define PRINT_INTERVAL_CYCLES (SAMPLING_FREQ_HZ / PRINT_FREQUENCY_HZ)
#define GBIAS_ACC_TH_SC (2.0f * 0.000765f)
#define GBIAS_GYRO_TH_SC (2.0f * 0.002f)
#define GBIAS_MAG_TH_SC (2.0f * 0.001500f)
#define DECIMATION 1U
#define MAG_CAL_DIVISOR 500.0f

/* Private variables ---------------------------------------------------------*/
static MFX_knobs_t MotionFX_knobs;
static MFX_input_t data_in;
static MFX_output_t data_out;
static uint8_t mfxstate[STATE_SIZE];
static MFX_MagCal_input_t mag_data_in_cal;
static MFX_MagCal_output_t mag_cal_out;

static AppState_t AppState = APP_STATE_CALIBRATING;
static uint32_t print_counter = 0;
static IKS02A1_MOTION_SENSOR_Axes_t mag_axes;

/* Private function prototypes -----------------------------------------------*/
static void MX_IKS02A1_DataLogTerminal_Init(void);
static void MX_IKS02A1_DataLogTerminal_Process(void);
static void initialize_motion_fx(void);
static void print_full_output(void);
static void print_calibration_status(void);

void MX_MEMS_Init(void)
{
 MX_IKS02A1_DataLogTerminal_Init();
}

void MX_MEMS_Process(void)
{
 MX_IKS02A1_DataLogTerminal_Process();
}

/**
 * @brief Initialize the application.
 */
void MX_IKS02A1_DataLogTerminal_Init(void)
{
 BSP_LED_Init(LED2);
 BSP_PB_Init(BUTTON_KEY, BUTTON_MODE_EXTI);
 BSP_COM_Init(COM1);

 printf("-- STMicroelectronics JMX MotionFX Fusion DEMO --\r\n");

 IKS02A1_MOTION_SENSOR_Init(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO | MOTION_GYRO);
 IKS02A1_MOTION_SENSOR_Init(IKS02A1_IIS2MDC_0, MOTION_MAGNETO);
 IKS02A1_MOTION_SENSOR_Enable(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO);
 IKS02A1_MOTION_SENSOR_Enable(IKS02A1_ISM330DHCX_0, MOTION_GYRO);
 IKS02A1_MOTION_SENSOR_Enable(IKS02A1_IIS2MDC_0, MOTION_MAGNETO);
 printf("Programando valores de Rango para ISM330DHCX Gyro/Acc...\r\n");
 IKS02A1_MOTION_SENSOR_SetFullScale(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO, 4);
 IKS02A1_MOTION_SENSOR_SetFullScale(IKS02A1_ISM330DHCX_0, MOTION_GYRO, 500);
 int32_t fs_acc;
 int32_t fs_gyro;
 IKS02A1_MOTION_SENSOR_GetFullScale(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO, &fs_acc);
 IKS02A1_MOTION_SENSOR_GetFullScale(IKS02A1_ISM330DHCX_0, MOTION_GYRO, &fs_gyro);
 printf("Accelerometer FSR set to: %ld g\r\n", fs_acc);
 printf("Gyroscope FSR set to: %ld dps\r\n", fs_gyro);


 IKS02A1_MOTION_SENSOR_SetOutputDataRate(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO, SAMPLING_FREQ_HZ);
 IKS02A1_MOTION_SENSOR_SetOutputDataRate(IKS02A1_ISM330DHCX_0, MOTION_GYRO, SAMPLING_FREQ_HZ);
 IKS02A1_MOTION_SENSOR_SetOutputDataRate(IKS02A1_IIS2MDC_0, MOTION_MAGNETO, SAMPLING_FREQ_HZ);

 initialize_motion_fx();
}

/**
 * @brief Main application process.
 */
void MX_IKS02A1_DataLogTerminal_Process(void)
{
 IKS02A1_MOTION_SENSOR_Axes_t acc_axes, gyro_axes;
 float delta_time = (float)SAMPLING_PERIOD_MS / 1000.0f;

 IKS02A1_MOTION_SENSOR_GetAxes(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO, &acc_axes);
 IKS02A1_MOTION_SENSOR_GetAxes(IKS02A1_ISM330DHCX_0, MOTION_GYRO, &gyro_axes);
 IKS02A1_MOTION_SENSOR_GetAxes(IKS02A1_IIS2MDC_0, MOTION_MAGNETO, &mag_axes);

 data_in.acc[0] = acc_axes.x / 1000.0f;
 data_in.acc[1] = acc_axes.y / 1000.0f;
 data_in.acc[2] = acc_axes.z / 1000.0f;

 data_in.gyro[0] = gyro_axes.x / 1000.0f;
 data_in.gyro[1] = gyro_axes.y / 1000.0f;
 data_in.gyro[2] = gyro_axes.z / 1000.0f;

 if (AppState == APP_STATE_CALIBRATING)
 {
 // Durante la calibración, alimentar la utilidad MagCal con datos en uT/50
 mag_data_in_cal.mag[0] = mag_axes.x / MAG_CAL_DIVISOR;
 mag_data_in_cal.mag[1] = mag_axes.y / MAG_CAL_DIVISOR;
 mag_data_in_cal.mag[2] = mag_axes.z / MAG_CAL_DIVISOR;
 mag_data_in_cal.time_stamp = HAL_GetTick();
 MotionFX_MagCal_run(&mag_data_in_cal);

 print_calibration_status();
 MotionFX_MagCal_getParams(&mag_cal_out);

 if (mag_cal_out.cal_quality == MFX_MAGCALGOOD)
 {
 printf("\r\n--- CALIBRACION COMPLETA! ---\r\n");
 printf("Iniciando salida de datos de fusion...\r\n\r\n");
 AppState = APP_STATE_RUNNING;
 }
 }
 else if (AppState == APP_STATE_RUNNING)
 {

 data_in.mag[0] = (mag_axes.x / MAG_CAL_DIVISOR) - mag_cal_out.hi_bias[0];
 data_in.mag[1] = (mag_axes.y / MAG_CAL_DIVISOR) - mag_cal_out.hi_bias[1];
 data_in.mag[2] = (mag_axes.z / MAG_CAL_DIVISOR) - mag_cal_out.hi_bias[2];
 MotionFX_propagate((MFXState_t *)mfxstate, &data_out, &data_in, &delta_time);
 MotionFX_update((MFXState_t *)mfxstate, &data_out, &data_in, &delta_time, NULL);

 print_counter++;
 if (print_counter >= PRINT_INTERVAL_CYCLES)
 {
 print_full_output();
 print_counter = 0;
 }
 }

 HAL_Delay(SAMPLING_PERIOD_MS);
}

/**
 * @brief Initialize the MotionFX library and configure knobs.
 */
static void initialize_motion_fx(void)
{
 __HAL_RCC_CRC_CLK_ENABLE();
 MotionFX_initialize((MFXState_t *)mfxstate);

 MotionFX_getKnobs((MFXState_t *)mfxstate, &MotionFX_knobs);

 BSP_SENSOR_ACC_GetOrientation(MotionFX_knobs.acc_orientation);
 BSP_SENSOR_GYR_GetOrientation(MotionFX_knobs.gyro_orientation);
 BSP_SENSOR_MAG_GetOrientation(MotionFX_knobs.mag_orientation);

 MotionFX_knobs.gbias_acc_th_sc = GBIAS_ACC_TH_SC;
 MotionFX_knobs.gbias_gyro_th_sc = GBIAS_GYRO_TH_SC;
 MotionFX_knobs.gbias_mag_th_sc = GBIAS_MAG_TH_SC;
 MotionFX_knobs.LMode = 1;
 MotionFX_knobs.modx = DECIMATION;
 MotionFX_knobs.output_type = MFX_ENGINE_OUTPUT_ENU;
 MotionFX_knobs.ATime = 0.2f;
 MotionFX_knobs.MTime = 0.1f;



 MotionFX_setKnobs((MFXState_t *)mfxstate, &MotionFX_knobs);

 printf("Orientations -> ACC:%s, GYR:%s, MAG:%s\r\n",
 MotionFX_knobs.acc_orientation,
 MotionFX_knobs.gyro_orientation,
 MotionFX_knobs.mag_orientation);
 printf("Fusion output type -> %s\r\n",
 (MotionFX_knobs.output_type == MFX_ENGINE_OUTPUT_ENU) ? "ENU" : "NED");

 MotionFX_enable_9X((MFXState_t *)mfxstate, MFX_ENGINE_ENABLE);

 MotionFX_MagCal_init(SAMPLING_PERIOD_MS, 1);

 printf("Slowly rotate the board in a figure-8 pattern to calibrate the magnetometer.\r\n\r\n");
}

/**
 * @brief Print the full fused data output and diagnostic info.
 */
static void print_full_output(void)
{
 float quat_q0 = data_out.quaternion[0];
 float quat_q1 = data_out.quaternion[1];
 float quat_q2 = data_out.quaternion[2];
 float quat_q3 = data_out.quaternion[3];

 float rot_yaw = data_out.rotation[0];
 float rot_pitch = data_out.rotation[1];
 float rot_roll = data_out.rotation[2];

 float g_x = data_out.gravity[0];
 float g_y = data_out.gravity[1];
 float g_z = data_out.gravity[2];

 float la_x = data_out.linear_acceleration[0];
 float la_y = data_out.linear_acceleration[1];
 float la_z = data_out.linear_acceleration[2];

 float fused_heading = data_out.heading;
 float heading_error = data_out.headingErr;

 printf("Q(%.4f,%.4f,%.4f,%.4f) R(Y:%.4f,P:%.4f,R:%.4f) G_g(x:%.4f,y:%.4f,z:%.4f) LA_g(x:%.4f,y:%.4f,z:%.4f) H_error:%.3f Heading_Fused:%.2f\r\n",
 quat_q0, quat_q1, quat_q2, quat_q3,
 rot_yaw, rot_pitch, rot_roll,
 g_x, g_y, g_z,
 la_x, la_y, la_z,
		 heading_error, fused_heading);
}

/**
 * @brief Print only the magnetometer calibration status.
 */
static void print_calibration_status(void)
{
 MFX_MagCal_output_t mag_cal_out_local;
 MotionFX_MagCal_getParams(&mag_cal_out_local);

 MFX_MagCal_quality_t cal_quality = mag_cal_out_local.cal_quality;
 char *quality_str;
 switch(cal_quality)
 {
 case MFX_MAGCALUNKNOWN: quality_str = "UNKNOWN"; break;
 case MFX_MAGCALPOOR: quality_str = "POOR"; break;
 case MFX_MAGCALOK: quality_str = "OK"; break;
 case MFX_MAGCALGOOD: quality_str = "GOOD"; break;
 default: quality_str = "ERROR"; break;
 }

 printf("Calibrating... Quality: %s \r", quality_str);
}

#ifdef __cplusplus
}
#endif

3 replies

Associate II
July 15, 2025

Hello WrenchInTheWorks

 

Have you manage to get fusion values that are correct using the MotionFX library? like heading, Roll, Pitch, Yaw?

 

If yes how did you define this part:?

 

strcpy((char *)MotionFX_knobs.acc_orientation, "swu");
strcpy((char *)MotionFX_knobs.gyro_orientation, "swu");
strcpy((char *)MotionFX_knobs.mag_orientation, "enu");

 

and what sensor/board you are using?

 

Kind regards

 

JD

WrenchInTheWorks
Associate II
July 15, 2025

Hello @Pantera_MXJ,

I'm getting values for everything but Roll, Pitch, Yaw, unsure why, maybe because I have not set my orientation yet or because you may not get them in 6x mode, not sure . I've got bigger problems in my code base to deal with now that I know I can get values in out of the FX engine.

So to answer your first question I ignored that part (for now), I'll let you know once I get that sorted.

I'm using a custom board with the LSM6DSMTR.

Cheers,

Michael 

Associate II
July 15, 2025

Thank you! will wait for your feedback as I can't figure out how to set up my board correctly.

WrenchInTheWorks
Associate II
July 15, 2025

What board do you have? Can you share your code? I may be able to help.

 

Cheers, 

Michael 

Associate II
July 16, 2025

Hello WrenchInTheWorks

 

Thanks for the help! I have a IKS02A1 I had some progress but still some values are not ok, I think I'm close but something is wrong, I just added the code in the post I have related to this problem:

X-NUCLEO-IKS02A1 sensor orientation (axis) on PCB ... - STMicroelectronics Community

Kind regards.

JD

Federica Bossi
Federica BossiBest answer
Technical Moderator
July 28, 2025

Hi @Pantera_MXJ ,

I share also here the corrected code you posted on the other topic, so that if someone else in the future encounters the same issue can solve:

/**
 ******************************************************************************
 * File Name : app_mems.c
 * Description : This file provides code for the configuration
 * of the STMicroelectronics.X-CUBE-MEMS1.11.3.0 instances.
 ******************************************************************************
 * @attention
 *
 * JMX Fusion Terminal JUL 17 2025
 * 
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */

#ifdef __cplusplus
extern "C" {
#endif

/* Includes ------------------------------------------------------------------*/
#include "app_mems.h"
#include "main.h"
#include <stdio.h>
#include <string.h>

#define _USE_MATH_DEFINES
#include <math.h>

#include "iks02a1_motion_sensors.h"
#include "stm32u5xx_nucleo.h"
#include "motion_fx.h"
#include "iks02a1_mems_control_ex.h"

/* Private typedef -----------------------------------------------------------*/
typedef enum {
 APP_STATE_CALIBRATING,
 APP_STATE_RUNNING
} AppState_t;

/* Private define ------------------------------------------------------------*/
#define SAMPLING_FREQ_HZ 100
#define SAMPLING_PERIOD_MS (1000 / SAMPLING_FREQ_HZ)
#define STATE_SIZE (2450)
#define PRINT_FREQUENCY_HZ 5
#define PRINT_INTERVAL_CYCLES (SAMPLING_FREQ_HZ / PRINT_FREQUENCY_HZ)
#define GBIAS_ACC_TH_SC (2.0f * 0.000765f)
#define GBIAS_GYRO_TH_SC (2.0f * 0.002f)
#define GBIAS_MAG_TH_SC (2.0f * 0.001500f)
#define DECIMATION 1U
#define MAG_CAL_DIVISOR 500.0f

/* Private variables ---------------------------------------------------------*/
static MFX_knobs_t MotionFX_knobs;
static MFX_input_t data_in;
static MFX_output_t data_out;
static uint8_t mfxstate[STATE_SIZE];
static MFX_MagCal_input_t mag_data_in_cal;
static MFX_MagCal_output_t mag_cal_out;

static AppState_t AppState = APP_STATE_CALIBRATING;
static uint32_t print_counter = 0;
static IKS02A1_MOTION_SENSOR_Axes_t mag_axes;

/* Private function prototypes -----------------------------------------------*/
static void MX_IKS02A1_DataLogTerminal_Init(void);
static void MX_IKS02A1_DataLogTerminal_Process(void);
static void initialize_motion_fx(void);
static void print_full_output(void);
static void print_calibration_status(void);

void MX_MEMS_Init(void)
{
 MX_IKS02A1_DataLogTerminal_Init();
}

void MX_MEMS_Process(void)
{
 MX_IKS02A1_DataLogTerminal_Process();
}

/**
 * @brief Initialize the application.
 */
void MX_IKS02A1_DataLogTerminal_Init(void)
{
 BSP_LED_Init(LED2);
 BSP_PB_Init(BUTTON_KEY, BUTTON_MODE_EXTI);
 BSP_COM_Init(COM1);

 printf("-- STMicroelectronics JMX MotionFX Fusion DEMO --\r\n");

 IKS02A1_MOTION_SENSOR_Init(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO | MOTION_GYRO);
 IKS02A1_MOTION_SENSOR_Init(IKS02A1_IIS2MDC_0, MOTION_MAGNETO);
 IKS02A1_MOTION_SENSOR_Enable(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO);
 IKS02A1_MOTION_SENSOR_Enable(IKS02A1_ISM330DHCX_0, MOTION_GYRO);
 IKS02A1_MOTION_SENSOR_Enable(IKS02A1_IIS2MDC_0, MOTION_MAGNETO);
 printf("Programando valores de Rango para ISM330DHCX Gyro/Acc...\r\n");
 IKS02A1_MOTION_SENSOR_SetFullScale(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO, 4);
 IKS02A1_MOTION_SENSOR_SetFullScale(IKS02A1_ISM330DHCX_0, MOTION_GYRO, 500);
 int32_t fs_acc;
 int32_t fs_gyro;
 IKS02A1_MOTION_SENSOR_GetFullScale(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO, &fs_acc);
 IKS02A1_MOTION_SENSOR_GetFullScale(IKS02A1_ISM330DHCX_0, MOTION_GYRO, &fs_gyro);
 printf("Accelerometer FSR set to: %ld g\r\n", fs_acc);
 printf("Gyroscope FSR set to: %ld dps\r\n", fs_gyro);


 IKS02A1_MOTION_SENSOR_SetOutputDataRate(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO, SAMPLING_FREQ_HZ);
 IKS02A1_MOTION_SENSOR_SetOutputDataRate(IKS02A1_ISM330DHCX_0, MOTION_GYRO, SAMPLING_FREQ_HZ);
 IKS02A1_MOTION_SENSOR_SetOutputDataRate(IKS02A1_IIS2MDC_0, MOTION_MAGNETO, SAMPLING_FREQ_HZ);

 initialize_motion_fx();
}

/**
 * @brief Main application process.
 */
void MX_IKS02A1_DataLogTerminal_Process(void)
{
 IKS02A1_MOTION_SENSOR_Axes_t acc_axes, gyro_axes;
 float delta_time = (float)SAMPLING_PERIOD_MS / 1000.0f;

 IKS02A1_MOTION_SENSOR_GetAxes(IKS02A1_ISM330DHCX_0, MOTION_ACCELERO, &acc_axes);
 IKS02A1_MOTION_SENSOR_GetAxes(IKS02A1_ISM330DHCX_0, MOTION_GYRO, &gyro_axes);
 IKS02A1_MOTION_SENSOR_GetAxes(IKS02A1_IIS2MDC_0, MOTION_MAGNETO, &mag_axes);

 data_in.acc[0] = acc_axes.x / 1000.0f;
 data_in.acc[1] = acc_axes.y / 1000.0f;
 data_in.acc[2] = acc_axes.z / 1000.0f;

 data_in.gyro[0] = gyro_axes.x / 1000.0f;
 data_in.gyro[1] = gyro_axes.y / 1000.0f;
 data_in.gyro[2] = gyro_axes.z / 1000.0f;

 if (AppState == APP_STATE_CALIBRATING)
 {
 // Durante la calibración, alimentar la utilidad MagCal con datos en uT/50
 mag_data_in_cal.mag[0] = mag_axes.x / MAG_CAL_DIVISOR;
 mag_data_in_cal.mag[1] = mag_axes.y / MAG_CAL_DIVISOR;
 mag_data_in_cal.mag[2] = mag_axes.z / MAG_CAL_DIVISOR;
 mag_data_in_cal.time_stamp = HAL_GetTick();
 MotionFX_MagCal_run(&mag_data_in_cal);

 print_calibration_status();
 MotionFX_MagCal_getParams(&mag_cal_out);

 if (mag_cal_out.cal_quality == MFX_MAGCALGOOD)
 {
 printf("\r\n--- CALIBRACION COMPLETA! ---\r\n");
 printf("Iniciando salida de datos de fusion...\r\n\r\n");
 AppState = APP_STATE_RUNNING;
 }
 }
 else if (AppState == APP_STATE_RUNNING)
 {

 data_in.mag[0] = (mag_axes.x / MAG_CAL_DIVISOR) - mag_cal_out.hi_bias[0];
 data_in.mag[1] = (mag_axes.y / MAG_CAL_DIVISOR) - mag_cal_out.hi_bias[1];
 data_in.mag[2] = (mag_axes.z / MAG_CAL_DIVISOR) - mag_cal_out.hi_bias[2];
 MotionFX_propagate((MFXState_t *)mfxstate, &data_out, &data_in, &delta_time);
 MotionFX_update((MFXState_t *)mfxstate, &data_out, &data_in, &delta_time, NULL);

 print_counter++;
 if (print_counter >= PRINT_INTERVAL_CYCLES)
 {
 print_full_output();
 print_counter = 0;
 }
 }

 HAL_Delay(SAMPLING_PERIOD_MS);
}

/**
 * @brief Initialize the MotionFX library and configure knobs.
 */
static void initialize_motion_fx(void)
{
 __HAL_RCC_CRC_CLK_ENABLE();
 MotionFX_initialize((MFXState_t *)mfxstate);

 MotionFX_getKnobs((MFXState_t *)mfxstate, &MotionFX_knobs);

 BSP_SENSOR_ACC_GetOrientation(MotionFX_knobs.acc_orientation);
 BSP_SENSOR_GYR_GetOrientation(MotionFX_knobs.gyro_orientation);
 BSP_SENSOR_MAG_GetOrientation(MotionFX_knobs.mag_orientation);

 MotionFX_knobs.gbias_acc_th_sc = GBIAS_ACC_TH_SC;
 MotionFX_knobs.gbias_gyro_th_sc = GBIAS_GYRO_TH_SC;
 MotionFX_knobs.gbias_mag_th_sc = GBIAS_MAG_TH_SC;
 MotionFX_knobs.LMode = 1;
 MotionFX_knobs.modx = DECIMATION;
 MotionFX_knobs.output_type = MFX_ENGINE_OUTPUT_ENU;
 MotionFX_knobs.ATime = 0.2f;
 MotionFX_knobs.MTime = 0.1f;



 MotionFX_setKnobs((MFXState_t *)mfxstate, &MotionFX_knobs);

 printf("Orientations -> ACC:%s, GYR:%s, MAG:%s\r\n",
 MotionFX_knobs.acc_orientation,
 MotionFX_knobs.gyro_orientation,
 MotionFX_knobs.mag_orientation);
 printf("Fusion output type -> %s\r\n",
 (MotionFX_knobs.output_type == MFX_ENGINE_OUTPUT_ENU) ? "ENU" : "NED");

 MotionFX_enable_9X((MFXState_t *)mfxstate, MFX_ENGINE_ENABLE);

 MotionFX_MagCal_init(SAMPLING_PERIOD_MS, 1);

 printf("Slowly rotate the board in a figure-8 pattern to calibrate the magnetometer.\r\n\r\n");
}

/**
 * @brief Print the full fused data output and diagnostic info.
 */
static void print_full_output(void)
{
 float quat_q0 = data_out.quaternion[0];
 float quat_q1 = data_out.quaternion[1];
 float quat_q2 = data_out.quaternion[2];
 float quat_q3 = data_out.quaternion[3];

 float rot_yaw = data_out.rotation[0];
 float rot_pitch = data_out.rotation[1];
 float rot_roll = data_out.rotation[2];

 float g_x = data_out.gravity[0];
 float g_y = data_out.gravity[1];
 float g_z = data_out.gravity[2];

 float la_x = data_out.linear_acceleration[0];
 float la_y = data_out.linear_acceleration[1];
 float la_z = data_out.linear_acceleration[2];

 float fused_heading = data_out.heading;
 float heading_error = data_out.headingErr;

 printf("Q(%.4f,%.4f,%.4f,%.4f) R(Y:%.4f,P:%.4f,R:%.4f) G_g(x:%.4f,y:%.4f,z:%.4f) LA_g(x:%.4f,y:%.4f,z:%.4f) H_error:%.3f Heading_Fused:%.2f\r\n",
 quat_q0, quat_q1, quat_q2, quat_q3,
 rot_yaw, rot_pitch, rot_roll,
 g_x, g_y, g_z,
 la_x, la_y, la_z,
		 heading_error, fused_heading);
}

/**
 * @brief Print only the magnetometer calibration status.
 */
static void print_calibration_status(void)
{
 MFX_MagCal_output_t mag_cal_out_local;
 MotionFX_MagCal_getParams(&mag_cal_out_local);

 MFX_MagCal_quality_t cal_quality = mag_cal_out_local.cal_quality;
 char *quality_str;
 switch(cal_quality)
 {
 case MFX_MAGCALUNKNOWN: quality_str = "UNKNOWN"; break;
 case MFX_MAGCALPOOR: quality_str = "POOR"; break;
 case MFX_MAGCALOK: quality_str = "OK"; break;
 case MFX_MAGCALGOOD: quality_str = "GOOD"; break;
 default: quality_str = "ERROR"; break;
 }

 printf("Calibrating... Quality: %s \r", quality_str);
}

#ifdef __cplusplus
}
#endif
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.