Skip to main content
SAbba.1
Associate III
May 23, 2023
Solved

Timeout when i try to overwrite apps on SensorTile.BOX (Entry Mode)

  • May 23, 2023
  • 5 replies
  • 3066 views

Estoy probando el SensorTile.box y he intentando reiteradas veces probar alguna de las aplicaciones que ya están diseñadas, he intentado en IOS y se queda cargando el overwrite y nunca termina, y he probado en Andriod y me da un error de Timeout.

¿Alguien sabe lo que me está pasando? 

He probado conectar y desconectar la bateria, intente con varios telefonos y probe apagando y encendiendo la placa

    This topic has been closed for replies.
    Best answer by Federica Bossi

    Hi @Sergio Abbattista Hernández​ ,

    The procedure is the one you find from pag 56 to 66.

    Please try to reset the board in this way and let me know if this solves the issue.

    In case this solves your problem, please mark my answer as "Best Answer" by clicking on the "Select as Best" button, this can be helpful for Community users to find this solution faster :)

    5 replies

    Federica Bossi
    Technical Moderator
    May 23, 2023

    Hi @Sergio Abbattista Hernández​ ,

    Welcome to ST Community!

    Which android and IOS version are you using? Which phone do you have? and which Firmware version are you adopting?

    Thanks

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
    SAbba.1
    SAbba.1Author
    Associate III
    May 23, 2023

    I have an iphone 13 and the IOS version is 16.1.1, however, I think I found the problem.

    This board was being used by someone before, so I guess it will have a FW that does not allow me to use the app properly.

    So I think the solution is to factory reset the board, which I guess will be by putting the base FW.

    If you know how I can do it, or if this could be my problem I would appreciate it, I have found this (page 56)

    SAbba.1
    SAbba.1Author
    Associate III
    May 23, 2023

    I want to remember that for the moment I want to use the ENTRY mode of the tilebox (not the EXPERT or PRO mode), because I want to get familiar with the capabilities of this board.

    Federica Bossi
    Federica BossiBest answer
    Technical Moderator
    May 23, 2023

    Hi @Sergio Abbattista Hernández​ ,

    The procedure is the one you find from pag 56 to 66.

    Please try to reset the board in this way and let me know if this solves the issue.

    In case this solves your problem, please mark my answer as "Best Answer" by clicking on the "Select as Best" button, this can be helpful for Community users to find this solution faster :)

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
    SAbba.1
    SAbba.1Author
    Associate III
    May 28, 2023

    ty, it works

    SAbba.1
    SAbba.1Author
    Associate III
    May 23, 2023

    perfect, i will try tonight or maybe tomorrow