Skip to main content
LCari.1
Associate
November 2, 2022
Solved

Using the STEVAL-MKI109V3 with MKI179V1 accelerometer daugther board, connected to PC via USB Lauching Unico GUI 9.13.0.0 and selecting a device -> communication error probably due to an unappropriate driver What driver is to be used with Windows 10?

  • November 2, 2022
  • 9 replies
  • 3019 views

..

This topic has been closed for replies.
Best answer by LCari.1

Hello ,

Yes for both.

In the meantime, I have installed the following : VCP_V1.5.0_Setup_W8_x64_64bits.exe and it works now.

But, normally I should not have done this according to STm video "Getting started with profiMEMS" explaining needed driver are already native in the files.zip

9 replies

Eleon BORLINI
ST Employee
November 3, 2022

Hi @LCari.1​ ,

can you see the STM32 board in the device manager?

And did you uploaded the last firmware update on the STEVAL-MKI109V3?

-Eleon

LCari.1
LCari.1AuthorBest answer
Associate
November 3, 2022

Hello ,

Yes for both.

In the meantime, I have installed the following : VCP_V1.5.0_Setup_W8_x64_64bits.exe and it works now.

But, normally I should not have done this according to STm video "Getting started with profiMEMS" explaining needed driver are already native in the files.zip

Eleon BORLINI
ST Employee
November 3, 2022

Those are the win8 drivers, the win10 has already embedded the STM32 drivers... or at least it should

-Eleon

LCari.1
LCari.1Author
Associate
November 3, 2022

Yes that 's what I understood as well. no need for W10

BUT, it didn't work , the port was enumeraed in Device Manager but no way to communicate....

LCari.1
LCari.1Author
Associate
November 3, 2022

By the way, I have posted another issue on the web case 00167097:

I have downloaded the UNICO GUI software to develop an apps using the accelerometer ref = LIS2DW12 with the STEVAL-MKI109V3 (Professional MEMS tool).

When clicking on the <Advanced Features> in option tab , the "current supply measurement / power supply" window does not pop up. No way to measure the current which is the basics.... Moreover, it enters in an never ending loop with UNICO is not responding !

Could you help on that one ?

Thanks

LCari.1
LCari.1Author
Associate
November 3, 2022

coming back to FW version: I have V2.18.6 coming with download of GUI UNICO V9.13.0.0.

Is it correct?

In the UM1049 I read 3.30.0

Eleon BORLINI
ST Employee
November 3, 2022

Hi @LCari.1​ ,

the associated Unico FW should be the v 3.42.4 version

0693W00000VOqDxQAL.png-Eleon

LCari.1
LCari.1Author
Associate
November 3, 2022

Yes , I have the V3.42.4

0693W00000VOqF0QAL.png

Eleon BORLINI
ST Employee
November 4, 2022

And did you uploaded it on the ProfiMEMS?

LCari.1
LCari.1Author
Associate
November 4, 2022

Eventually I have updated , more than painful, the STEVAL-MKI109V3 (DFU) and now the FW rev = V3.42.4 is installed. I can see the correct rev on UNICO GUI and everything works fine.

My point: I don't understand why downloading the last rev of UNICO GUI from the website then lauching the corresponding .exe there is no automatic check on the STEVAL board of its current implemented FW rev to see if there is a match....

Any comment ?

LCari.1
LCari.1Author
Associate
November 3, 2022

The interface has many less tabs and options than the on described in the UM1049

0693W00000VOqFtQAL.png 

Eleon BORLINI
ST Employee
November 4, 2022

It should be related to the fact that you are using a pure accelerometer, the LIS2DW12. On this device, differently for example from 6-axis IMUs (e.g. LSM6DSOX), you don't have digital features such as the FSM, the MLC, etc...

-Eleon

LCari.1
LCari.1Author
Associate
November 4, 2022

Yes but for the mother board itself STEVAL-MKI109V3 ,I should have got the rev 3.42.4, correct?

0693W00000VOtBVQA1.png