Skip to main content
Associate II
April 2, 2024
Question

Using X-CUBE-MEMSMIC1 without X-NUCLEO-CCA02M1

  • April 2, 2024
  • 2 replies
  • 1429 views

Hello, I am trying to record audio with external digital PDM microphones using the MEMSMIC1 example but it is not so straightforward without the nucleo expansion board. Because the CCA02M1 has a direct connection to the pc it is able to be detected as a microphone in the device manager, it is easily used through audacity. How can I implement this project and use audacity with my microphone setup if they are directly connected only to the development board (I am using nucleo-wb55rg)?

2 replies

SimonePradolini
Technical Moderator
April 5, 2024

Hello @greenthumb 

CCA02M1 can't work without STM32. It is mandatory to connect the X-NUCLEO to the NUCLEO board.

Furthermore, NUCLEO-WB55RG has not equipped with any microphone, so it can't work as a USB misrophone without CCA02M1.

It is not clear to me which setup would you like to use. Can you better explain it?

 

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
April 5, 2024

Hi Simone,

Thank you for your reply.

My setup is with an independent microphone attached to the nucleo-wb55rg. Hence why I say I want to use the memsmic1 example without the cca02m1, because the example is normally based off of that setup. So i'm trying to apply the example with the im73d122 digital microphones, preferable with the PDM interface. I guess start with one microphone but ideally end up using five.

Thank you!

Best,

Maia.

Associate II
January 28, 2026

Hey, did you get the solution, it would be a great help if you explain it to me as well because I am also trying to do something similar but with an external analog microphone.