Values for lm6dsox acc values in non movement state?
Hello
Im using steval mksbox 1vs1 for vibration analysis. I have taken measurements with motor in movement and withe the motor stopped. At first I supose that with the motor in stop mode, the acc values in the 3 axis should be near to 0.
In other thread I read that "You should at least see some differences between x and z axis when the device is flat on a surface (x almost close to 0, y almost close to 1g)."
Can you tell me which should be the normal values for the lm6dsox when there is no movement?
Thank you