Skip to main content
Associate
January 20, 2026
Solved

Vibration on the ISM330DHCX example or configuration using C driver

  • January 20, 2026
  • 2 replies
  • 197 views

I just like to configure the ISM330DHCX for vibration measurement. Is that an example or a sample code(using its C driver ) of it somewhere. Please give me a pointer. Thanks.

Best answer by Federica Bossi

Hi @ttron ,

You can look at our official driver on Github.

Hope this helps :)

2 replies

ttronAuthor
Associate
January 20, 2026

Let me expand on that: able to

1. Set a desire ODR

2. Set a threshold to wake up or trigger an interrupt (INT1). That's generate an interrupt if the acceleration above certain threshold (like > 10mg, etc).

3. Use stream FIFO

 

 

Andrew Neil
Super User
January 20, 2026
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Federica Bossi
Federica BossiBest answer
Technical Moderator
February 9, 2026

Hi @ttron ,

You can look at our official driver on Github.

Hope this helps :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.