Skip to main content
NSemrHomeInit
Associate III
March 23, 2023
Solved

What is the purpose of VDDIO in ISM330DLC Accelerometer

  • March 23, 2023
  • 2 replies
  • 1963 views

Dear ST,

I am using the ISM330DLC gyro and accelerometer,

In the electrical connection mode 1 I have a pin called VDDIO.

In my application I connected this pin to 3V but, I don't have any idea what is the use of this pin?

Thank you for explaining

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Well, that's in the data sheet, table 1, with the pin descriptions:

    VDDIO(1) Power supply for I/O pins

    Footnote 1 stands for: Recommended 100 nF filter capacitor.

    Does it answer your question?

    Regards

    /Peter

    2 replies

    Peter BENSCH
    Peter BENSCHBest answer
    Technical Moderator
    March 23, 2023

    Well, that's in the data sheet, table 1, with the pin descriptions:

    VDDIO(1) Power supply for I/O pins

    Footnote 1 stands for: Recommended 100 nF filter capacitor.

    Does it answer your question?

    Regards

    /Peter

    NSemrHomeInit
    Associate III
    March 23, 2023

    Hello Peter,

    I think that means If I want 4.5v on INT1/2, went the interrupt is triggered, I have to connect VIO to 4.5v?

    Peter BENSCH
    Technical Moderator
    March 23, 2023

    The data sheet clearly states in Table 3:

    Vdd_IO = Power supply for I/O, min 1.62V, max 3.6 V

    4.5V are slightly above 3.6V, so they are not permitted.

    If you need a different voltage level because the connected components work there, you still have to keep within the voltage range for VDDIO and use a level shifter at INT1 or INT2, for example.

    Regards

    /Peter