Skip to main content
Joerg Wagner
Senior III
February 13, 2025
Solved

X-CUBE-MEMSMIC1 : libhs_datalog.so for Raspberry Pi 5 or source code available?

  • February 13, 2025
  • 1 reply
  • 696 views

@SimonePradolini 

Hi Simone,

Can I get a 64 Bit version of libhs_datalog.so for Raspberry Pi 5 of the X-CUBE-MEMSMIC1 expansion software package please?

Or the source code to compile it?

Unfortunately DATALOG_V1.5.1 just provides a 32 Bit version libhs_datalog_rpi3b.so for Raspberry Pi 3B only.

This would be awesome.

 

Best regards

Joerg

Best answer by SimonePradolini

Hello @Joerg Wagner 

DATALOG1 is a bit old and there’s no plan for further major updates nor new board/host support.

Here you can find the most recent version available for libhs_datalog.so from DATALOG2. It’s 1 year old and it has been tested onto a Raspberry 4 64-bit O, but I wish it could work onto a Raspberry 5 also.

 

Let me know if it works properly on your setup.

Best regards,

Simone

1 reply

SimonePradolini
SimonePradoliniBest answer
Technical Moderator
February 14, 2025

Hello @Joerg Wagner 

DATALOG1 is a bit old and there’s no plan for further major updates nor new board/host support.

Here you can find the most recent version available for libhs_datalog.so from DATALOG2. It’s 1 year old and it has been tested onto a Raspberry 4 64-bit O, but I wish it could work onto a Raspberry 5 also.

 

Let me know if it works properly on your setup.

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.