Skip to main content
TYAMA.2
Associate II
December 23, 2021
Solved

About the recommended value of Cin of LDK320

  • December 23, 2021
  • 5 replies
  • 2178 views

About Cin of LDK320

What is the manufacturer's recommended value

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Welcome, @TYAMA.2​, to the community!

    Cin is not critical, but should have at least 1µF. You can use electrolytic capacitors, tantalum or MLCC.

    I would recommend a value between 1...10µF and position it as close as possible to the VIN pin.

    If this problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    5 replies

    Peter BENSCH
    Peter BENSCHBest answer
    Technical Moderator
    December 23, 2021

    Welcome, @TYAMA.2​, to the community!

    Cin is not critical, but should have at least 1µF. You can use electrolytic capacitors, tantalum or MLCC.

    I would recommend a value between 1...10µF and position it as close as possible to the VIN pin.

    If this problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    TYAMA.2
    TYAMA.2Author
    Associate II
    December 24, 2021

    Thank you for your reply.

    What is the effective value of the capacity of the capacitor in this case?

    Peter BENSCH
    Technical Moderator
    January 3, 2022

    I do not understand the question.

    Which case are you talking about and which capacitor do you mean?

    Regards

    /Peter

    TYAMA.2
    TYAMA.2Author
    Associate II
    February 28, 2022

    About Cin

    When considering temperature characteristics, DC bias characteristics, etc.

    How many μF or more do you need?

    Peter BENSCH
    Technical Moderator
    February 28, 2022

    As already mentioned: I would recommend a value between 1...10µF and position it as close as possible to the VIN pin.

    Regards

    /Peter

    TYAMA.2
    TYAMA.2Author
    Associate II
    March 2, 2022

    Is 1uF or more a value that takes DC bias characteristics and temperature characteristics into consideration?

    Or is it the standard value on the data sheet?

    Peter BENSCH
    Technical Moderator
    March 2, 2022

    The recommended value of 1...10µF is considered the current effective value. Depending on the respective technology used to manufacture the capacitor and thus on the specified capacitor parameters, the development engineer should of course select the correct values.

    If, for example, you already have a maximum tolerance of 50% over the temperature range, you have to use at least 2µF.

    TYAMA.2
    TYAMA.2Author
    Associate II
    March 2, 2022

    I understand.

    Thank you very much.