Skip to main content
vitor1
Associate II
September 14, 2016
Question

Application note x eDesign (Viper 26LD)

  • September 14, 2016
  • 3 replies
  • 2270 views
Posted on September 14, 2016 at 11:29

I have used eDesign for a buck converter design approach (see attachment). However, I noticed that the suggested components value are not the same as the ones on 

http://www.st.com/content/ccc/resource/technical/document/application_note/e6/81/42/cf/74/28/4f/78/DM00127577.pdf/files/DM00127577.pdf/jcr:content/translations/en.DM00127577.pdf

. What is the reason for the differences (especially at the compensation)?

Thanks in advance for your support.
This topic has been closed for replies.

3 replies

vitor1
vitor1Author
Associate II
September 22, 2016
Posted on September 22, 2016 at 08:45

Dear moderator,

Could you please give a support on this issue? It is quite important as I am going to a mass production soon.

Thanks for your understanding & support!

Patrizia Bellitto

Patrizia BELLITTO
ST Employee
September 22, 2016
Posted on September 22, 2016 at 09:43

Hello,

I forwarded your question to the application engineer a week ago, I'll reply as soon as he gives me some feedback.

Thanks for your interest and patience!

vitor1
vitor1Author
Associate II
December 13, 2016
Posted on December 13, 2016 at 13:32

Hello Patrizia,

Have you heard back from your application engineer? I have been waiting a long time for this feedback.

Thanks for your understanding!

Patrizia BELLITTO
ST Employee
December 14, 2016
Posted on December 14, 2016 at 10:00

Hello,

sorry, you are right...Could you tell me exactly the specification of your application?

Because the application note you pointed out expects two outputs, while eDesign allows only one.

Thanks

Patrizia

vitor1
vitor1Author
Associate II
December 14, 2016
Posted on December 14, 2016 at 10:21

Hi,

Yes, the one that I pointed out has 2 outputs but it should make a big difference on the design as for the 5V output a linear regulator is used. So, my understanding is that I should have a similar design (on eDesign) if I would use the same specification as STEVAL-ISA116V1 for the 16V.

I am looking forward to hearing from you.

Regards,