Skip to main content
theo kretzschmar-schuldorff
Associate
November 8, 2021
Question

Cannot issue NMEA commands to the Teseo on STEVAL-STRKT01 over good CN503 UART link.

  • November 8, 2021
  • 2 replies
  • 2532 views

Hello ST,

I’m attempting to integrate the STEVAL-STRKT01 into my system.

I need to issue NMEA commands to the Teseo .

I’m connected into the UART over CN503 (TX,RX,GND only) and I can see the serial chatter.

For example, I want to Stop the STAGPS engine with $PSTMSTAGPSONOFF,0*4A

This, and all other commands I am testing, are getting no responses. Am I doing something wrong, or can I not send NMEA to the Teseo on this Evaluation board?

Attached a screenshot of one of the billion ways I’ve tried this. Any help much appreciated!

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    November 8, 2021

    How about a simpler firmware version query?

    Any inbound commands work?

    TESEO-SUITE ?

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    theo kretzschmar-schuldorff
    Associate
    November 8, 2021

    Its hard to tell if my NMEA commands are triggering any response at all, the UART is sporadically spooling out NMEA messages info without being prompted. Including versioning info.

    I suspect the STEVAL-STRKT01 board is continuously interrogating the Teseo and has exclusive use?

    I set up the Teseo-suite, image attached, but still couldn't get it to accept PSTMSTAGPSONOFF..

    Tesla DeLorean
    Guru
    November 9, 2021

    Would check you're not getting some conflicting signals on the GPS's RX pin from the LoRa MCU, or other sources/connections.

    https://www.st.com/resource/en/schematic_pack/steval-strkt01_schematic.pdf

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    theo kretzschmar-schuldorff
    Associate
    November 9, 2021

    Thanks for your analysis - that's almost certainly right. The Lora module does seem to be obstructing my commands.

    Do you think I can hope to interrupt (temporarily) this UART connection between LoRa & LIV3 without damaging the hardware? I don't see an obvious move here..

    Tesla DeLorean
    Guru
    November 9, 2021

    I'd probably start by removing resistor/zero-ohm R204, so you can connect via TP202

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..