Skip to main content
mirko239955
Associate
September 14, 2011
Question

CANopen stack SPEAr320

  • September 14, 2011
  • 5 replies
  • 1145 views
Posted on September 14, 2011 at 10:13

I'm looking for a CANopen software stack that can be implemented 

with the BSP running under Linux on SPEAr320,

for a project with a client  in the process automation.

Any software available from ST or 3rd parties ?

Thank you in advance

Mirko
This topic has been closed for replies.

5 replies

hj_it
Associate II
September 17, 2011
Posted on September 17, 2011 at 22:25

Hello Mirko,

port GmbH at http://www.port.de offers a comercial CANopen stack which works with either can4linux or SocketCAN on Linux. Please check if one of these CAN drivers is available for the SPEAr320.

 

 Regards

    Heinz

hj_it
Associate II
September 17, 2011
Posted on September 17, 2011 at 22:29

Mirko

the exact link is

http://www.port.de/0564library

 Regards

    Heinz

mirko239955
Associate
September 19, 2011
Posted on September 19, 2011 at 12:02

Hi Heinz,

thank you for the infos.

i'm going to check it and come back to you asap.

Mirko 

myshanr
Visitor II
January 14, 2012
Posted on January 14, 2012 at 07:42

表示看�懂,呵呵。怎么ST论�那么冷清的

翻译:I don't know, ha ha. How to ST BBS so cold

scott23
Visitor II
May 22, 2016
Posted on May 22, 2016 at 13:18