Skip to main content
Mfathi50
Visitor II
August 12, 2022
Question

Case 1 5 GPS satellites with strong SNR & elevation angles above 10 degrees. Case 2 5 GPS satellites with a weak SNR & elevation angle above 10 degrees also. can case 2 be better than case 1 in positioning if the GDOP is better?

  • August 12, 2022
  • 1 reply
  • 647 views

..

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    August 12, 2022

    Once it has the navigation data, the SNR is less relevant.

    It tends to be most important to see the direct signals, not multi-path/reflected ones.

    The best solution is going to be the one with the least noisiest measurements.

    DOP tends to be assumed to be a multiplier for the CEP specification.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..