Skip to main content
ASing.20
Associate II
March 9, 2022
Question

Code gets stuck after enableInterrupts() and it does not function as per the logic.

  • March 9, 2022
  • 2 replies
  • 1504 views

#include "stm8l15x.h"

#include "stm8l15x_gpio.h"

#include "stm8l15x_exti.h"

#include "stm8l15x_rtc.h"

#include "stm8l15x_itc.h"

#include "stm8l15x_clk.h"

#define WAKEUP_GPIO_PORT    GPIOE

#define WAKEUP_GPIO_PORT    GPIOE

#define ICC_WAKEUP_GPIO_PIN   GPIO_Pin_6

static void RTC_Config(void)

{

 /* Configures the RTC */

 CLK_RTCClockConfig(CLK_RTCCLKSource_LSE, CLK_RTCCLKDiv_1);

 CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE);

  

 RTC_WakeUpClockConfig(RTC_WakeUpClock_CK_SPRE_16bits);

 RTC_ITConfig(RTC_IT_WUT, ENABLE);

 /* Enable Interrupts*/

  

}

void Delay(__IO uint32_t nCount)

{

 for (; nCount != 0; nCount--);

}

void main(void)

{

 GPIO_Init(GPIOC, GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);

GPIO_Init( WAKEUP_GPIO_PORT, ICC_WAKEUP_GPIO_PIN, GPIO_Mode_In_FL_IT);

/* Enable Rising edge port PE6 for wake up conter */

 EXTI->CR2 = 0x10; 

  /* RTC configuration -------------------------------------------*/

 RTC_Config();

enableInterrupts();

 /* Infinite loop */

 while (1)

 {

  GPIO_SetBits(GPIOC, GPIO_Pin_7);

  //Delay(0xFFFF);

   

  /* RTC will wake-up from halt every 5second */

  RTC_SetWakeUpCounter(5);

  RTC_WakeUpCmd(ENABLE);

  /* Enter Wait for interrupt mode*/

  wfi();

GPIO_ResetBits(GPIOC, GPIO_Pin_7);

Delay(60000);

  RTC_WakeUpCmd(DISABLE);

 }

}

    This topic has been closed for replies.

    2 replies

    AA1
    Senior III
    March 18, 2022

    After enable Interrupts, an interrupt occurs if any is active. Where is the ISR?

    And don't try to wakeup with GPIO and RTC at same time. Use just one, simplify you code.

    ASing.20
    ASing.20Author
    Associate II
    March 23, 2022

    Thanks, I got the solution.

    I was not using ISR after the interrupt that's why it used to get stuck.

    I have changed the ISR and now it's working fine.