Skip to main content
vinicius
Associate
August 17, 2015
Question

Difficulties in finding the ideal transformer

  • August 17, 2015
  • 5 replies
  • 1069 views
Posted on August 17, 2015 at 21:48

My first project using the tool eDesignSuite and I'm developing a switching power supply with a 85VAC to 265VAC input voltage with 24VDC output and 5A of output current. My difficulty is in finding the transformer to suit my application. Could someone help me?

This topic has been closed for replies.

5 replies

Patrizia BELLITTO
ST Employee
August 18, 2015
Posted on August 18, 2015 at 15:26

Hello,

I suppose you are using the L6566B/L6566BH to create a design with that output. 

eDesignSuite suggests an EER40, if you haven't modified any other parameters. Otherwise, could you give us more details?

Thanks in your interest in our tool.

 Best regards,

 Patrizia Bellitto

eDesignSuite development and support team

vinicius
viniciusAuthor
Associate
August 18, 2015
Posted on August 18, 2015 at 19:28

Hi, EER40 is the core. I wonder if you can help me with a commercial transformer, or if I really have to leave for a construction of a new transformer?

I'm using L6566B, and the only change I made was to change over current protection auto restart for current latched.

Patrizia BELLITTO
ST Employee
August 24, 2015
Posted on August 24, 2015 at 08:46

Hi,

Recently a list of commercial transformers from Wurth Elektronic was added to the list of core available in eDesignSuite.

From transformer design view, in the table where core type is shown, you can choose to ''Select from list'' another core, different from the one automatically suggested by eDesign.

According to your specifics, there is one commercial core from Wurth, ETD39 TH-H 16-Pin.

Could you please verify if it satisfies your requirements?

Best regards,

Patrizia

Patrizia BELLITTO
ST Employee
September 1, 2015
Posted on September 01, 2015 at 09:58

Hi,

according to your specs, there could be a Wurth commercial transformer suitable for your application. Its order code is 750811744, see attachment.

Please contact Emil Nierges, product applications engineer from WE<Emil.Nierges@we-online.com>, for further information.

Best regards,

Patrizia

________________

Attachments :

750811744.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyvI&d=%2Fa%2F0X0000000bIi%2FBmxKNkQJDmsGRP35g7KNMOvLRVciFU3fhY.h3BJ5Fec&asPdf=false
Emil Nierges
Visitor II
September 1, 2015
Posted on September 01, 2015 at 18:32

Dear Hillmann,

Indeed as Patrizia states, I made some research and I found a close solution for the transformer requirements in our database, see attached file: PN 750811744

We could provide samples to try them out and, even more, make a customs solution if needed based on electrical and mechanical requirements along with safety standard requirements.

Let me know your contact information so I can put you in touch with our local support.

Regards,

Emil Nierges

Product Applications Engineer

Wurth Electronics Midcom Inc.

emil.nierges@we-online.com

________________

Attachments :

750811744.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzEn&d=%2Fa%2F0X0000000bIj%2FEmKE2eq4sxiu8WSJzqS_XCLH61VsomaxsHM_28mJWW4&asPdf=false