Associate
January 23, 2025
Solved
ECMF02-4CMX8 - pin connection for USB type C application
- January 23, 2025
- 4 replies
- 1316 views
Hi,
I want to use ECMF02-4CMX8 as ESD protection and filtering means for a isolated USB 2.0 downstream port design.
The chosen connector is a Type C receptacle.
My question pertains to pin function of ECMF02-4CMX8.
The type C connector exposes two configuration pins, CC1 and CC2.
Can I connect CC1 to pin 4 and CC2 to pin 1 ?
From the datasheet I know the pin 1 is reserved to VBUS and pin 4 is reserved to ID, however I prefer to assign this 1 pin to CC2, and route VBUS to a separate over-voltage protection chip (MAX14699EWC+).
Is my choice correct and safe ?
I attach the proposed schematic for the complete interface.
Thank you for any help
Gabriele