Skip to main content
Gaston
Associate III
November 2, 2023
Solved

edesign does not fit with input specifications

  • November 2, 2023
  • 1 reply
  • 1634 views

Here's what eDesignSuite shows for a Boost DC/DC converter. The L7981 is a Buck converter so I don't understand the given results. Please anyone could clarify this?

Gaston_0-1698915085697.png

 

gaston

This topic has been closed for replies.
Best answer by Peter BENSCH

I am very sorry that the eDesign Suite displays this in a somewhat ambiguous way. STMicroelectronics does not have a boost regulator that can generate 24V from 13...18V without a circuit extension.

The L7981A is indeed a buck regulator, but like the other regulators shown (e.g. L7986A) it can be extended to a positive buck-boost with an external MOSFET. Such a regulator can then produce an output voltage that lies between the minimum and maximum input voltage, here e.g. 24V from 13...27V.

Hope that answers your question?

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
November 2, 2023

I am very sorry that the eDesign Suite displays this in a somewhat ambiguous way. STMicroelectronics does not have a boost regulator that can generate 24V from 13...18V without a circuit extension.

The L7981A is indeed a buck regulator, but like the other regulators shown (e.g. L7986A) it can be extended to a positive buck-boost with an external MOSFET. Such a regulator can then produce an output voltage that lies between the minimum and maximum input voltage, here e.g. 24V from 13...27V.

Hope that answers your question?

Regards
/Peter