Skip to main content
Central SUPPORT
Senior
March 27, 2019
Solved

EMI Filter for USB interface of STM32

  • March 27, 2019
  • 1 reply
  • 930 views

We are using USBUF01W6 as EMI filter for STM32F207VCT6 in USB D+ and D- lines in Full speed mode and we have connected VBUS (5V) at pin 3.3V pin of USBUF01W6.

Does this make sense to you?

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

This topic has been closed for replies.
Best answer by Central SUPPORT

As STM32 used already includes series resistors for USB D+ and D-, the right part to protect against ESD on D+ and D- is USBLC6-2SC6, instead of USBUF.

In addition, you should consider to protect 5V_USB against ESD and EOS transients (8/20µs). We recommend to use ESDA7P60-1U1M or ESDA7P120-1U1M. In this case, VBUS of USBLC6-2SC6 is connected to a 100nF capacitor or left open.

For best protection these parts should be placed as close as possible to the connector.

1 reply

Central SUPPORT
Central SUPPORTAuthorBest answer
Senior
March 27, 2019

As STM32 used already includes series resistors for USB D+ and D-, the right part to protect against ESD on D+ and D- is USBLC6-2SC6, instead of USBUF.

In addition, you should consider to protect 5V_USB against ESD and EOS transients (8/20µs). We recommend to use ESDA7P60-1U1M or ESDA7P120-1U1M. In this case, VBUS of USBLC6-2SC6 is connected to a 100nF capacitor or left open.

For best protection these parts should be placed as close as possible to the connector.