Skip to main content
Visitor II
January 9, 2024
Solved

Enquiry of availability of component for next 5 years as this will be used for New product design

  • January 9, 2024
  • 1 reply
  • 716 views

Enquiry of availability of component for next 5 years as this will be used for New product design


P/N: SM5908 . Is this product can be used for New product design? OR is it NRND?

 

THANK YOU

Best answer by Peter BENSCH

Welcome @ROOPA to the community!

Despite its advanced age (the TVS SM5908 has been on the market since 1999), there are currently no signs of it being discontinued. The global market still needs to protect its products against overvoltage, for which TVS with 1500W are perfectly suited. As it is also the only TVS for 5V and such power, it will almost certainly still be available in 2029 and beyond. However, this is my personal assessment and we cannot provide a written guarantee.

Hope that helps?

Good luck!
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
January 9, 2024

Welcome @ROOPA to the community!

Despite its advanced age (the TVS SM5908 has been on the market since 1999), there are currently no signs of it being discontinued. The global market still needs to protect its products against overvoltage, for which TVS with 1500W are perfectly suited. As it is also the only TVS for 5V and such power, it will almost certainly still be available in 2029 and beyond. However, this is my personal assessment and we cannot provide a written guarantee.

Hope that helps?

Good luck!
/Peter