Skip to main content
Associate
September 20, 2025
Solved

EVLSTGAP3SXS-H circuit question

  • September 20, 2025
  • 1 reply
  • 503 views

Hi,
Im analyzing the circuit of the STGAP3SXS in EVLSTGAP3SXS-.
I want to ask what's the purpose of this capacitance in the soft off pin, I thought it was filtering by why does it go to the VL instead of GND_ISO
Thank you.

Best answer by Peter BENSCH

It may be confusing, but C14 at the pin SOFTOFF is in fact a filter capacitor. However, in terms of AC, it is also connected to GNDISO_H via C9/C10, which are more than 30,000 times larger than C14, so that it performs its filter function in exactly the same way.

However, the DC reference point for the SOFTOFF output is VL, as can be clearly seen in section 6.5 of the data sheet, for example.

Hope that answers your question?

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
September 22, 2025

It may be confusing, but C14 at the pin SOFTOFF is in fact a filter capacitor. However, in terms of AC, it is also connected to GNDISO_H via C9/C10, which are more than 30,000 times larger than C14, so that it performs its filter function in exactly the same way.

However, the DC reference point for the SOFTOFF output is VL, as can be clearly seen in section 6.5 of the data sheet, for example.

Hope that answers your question?

Regards
/Peter