Skip to main content
Associate
May 5, 2025
Question

fail of MasterGan4

  • May 5, 2025
  • 1 reply
  • 651 views

I find the wavefrom of SW terminal(the connection of the bridge) is wrong. The frequency is consistent with the input signal but the Amplitude is 3V3. But there's no 3V3 power supply. It should have been the VIN I offer. And it's exactly a square wave. What may cause this case?

1 reply

Peter BENSCH
Technical Moderator
May 5, 2025

Welcome @ZHT, to the community!

Please forgive my lack of understanding, but the MASTERGAN4 has no terminal SW.

  • Could it be that you mean a ready-made board?
  • Is this board from STMicroelectronics, e.g. an evaluation board?

Regards
/Peter

ZHTAuthor
Associate
May 7, 2025

I'm sorry for the unclear description. Actually, I bought a chip MasterGan4TR and degisn the circuit with the reference of your evaluation board. Here's the specific circuit. The VIN input is 12V. I'm just confused about why it works abnormally like what I described before.

ZHT_0-1746594179147.png

 

 

Peter BENSCH
Technical Moderator
May 7, 2025

Well, the MASTERGAN4 is a half-bridge driver which usually handles up to 600V, but you want to operate use it with VIN at only 12V, right?

  • Please check whether VBO UVLO protection is already active.
  • Please also check at GH, where the gate of the HS GaN is led out, whether the drive level is sufficiently high and reaches at least 5V with respect to VOUT.

Regards
/Peter