Skip to main content
dv4
Associate
February 18, 2026
Solved

gdb dropped error, APs not closing, Fail reading CTRL/STAT register [Blue Pill]

  • February 18, 2026
  • 1 reply
  • 183 views

Title edited to flag that a Blue Pill is being used.


Info : [STN32F103c8Tx.cpu] Examination succeed
Info : starting gdb server for STN32F103C8Tx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Error:[STM32F103C8Tx.cpul clearing lockup after double fault Polling target STM32F103C8Tx.cpu failed, trying to reexamine Infò : (STM32F103C8Tx.cpu] cortex-M3 rlp1 processor detected
Info : [STN32F103c8Tx.cpuj target has 6 breakpoints, 4 watchpoints
Info :[STM32F103C8Tx.cpuj Examination succeed Info : accepting 'gdb' connection on tcp/3333Info : device id = 0x20036410
Info :flash size = 64 KiB
Info : accepting 'gdb' connection on tcp/3333
[STM32F103C8Tx.cpu] halted due to debug-request, current mode: Handler HardFault
XPSR: 0x21000003 pc: 0xfffffffe msp: 0x200008be
[STN32F103C8Tx.cpu] halted due to undefined, current mode: Thread XPSR: 0x61000000 pc: 0x2000003a msp: 0x200008b0.
Error: Fail reading CTRL/STAT register. Force reconnect
Info : dropped 'gdb' connection
Error: Fail reading CTRL/STAT register. Force reconnect
Error: [STM32F103C8Tx.cpu] not halted (gdb fileio)
Error:Fail reading CTRL/STAT register. Force reconnect
Polling target STN32F103C8Tx.cpu failed, trying to reexamine
Error: Fail reading CTRL/STAT register. Force reconnect
Erron:[STN32F103C8Tx.cpu] Examination failed
Examination failed, GDe will be halted. Polling again in 100ms
Error: Fail reading CTRL/STAT register, Force reconnect Error: Fail reading CTRL/STAT register. Force reconnect
Error: Failed to read memóry and, additionally, failed to find out where
shutdown command invoked
Info: dropped 'gdb'’ connection
Error: Error closing APs

Best answer by mƎALLEm

@dv4 wrote:
I am using a Blue Pill (STM32F103C8T6) development board. 

That could be an issue. As I said previously, for Blue Pill boards, most probably they contain a counterfeit chip.

 


@dv4 wrote:
 I am using an ST-Link V2

This one? (a post from @Andrew Neil from this knowledge base article:(

mALLEm_1-1771491103620.png

If yes, that could be also another problem.

So please use one of the ST boards that contains a genuine chip and STLINK.

You can purshase: the nucleo board: NUCLEO-F103RB

It contains a STM32F103 genuine chip as well as a genuine ST-LINK:

mALLEm_2-1771491269868.png

Hope that helps.

1 reply

mƎALLEm
Technical Moderator
February 19, 2026

Hello,

First, please review How to write your question to maximize your chances to find a solution.

Second, as "STM32F103C8T" is shown in the log, what board are you using? Blue Pill? If Blue Pull most probably the board contains a counterfeit chip.

What ST-LINK are you using? as there is a possibility you are using a cloned ST-LINK please read How to recognize a genuine ST-LINK/V2 versus a cloned one

What IDE Tool are you using? CubeIDE?

PS: from the trace:

Info : [STN32F103c8Tx.cpu] Examination succeed

That typo is a bit strange!

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
dv4
dv4Author
Associate
February 19, 2026
I am using a Blue Pill (STM32F103C8T6) development board. For software
development, I am working with STM32CubeMX and STM32CubeIDE. For
programming and debugging, I am using an ST-Link V2
mƎALLEm
mƎALLEmBest answer
Technical Moderator
February 19, 2026

@dv4 wrote:
I am using a Blue Pill (STM32F103C8T6) development board. 

That could be an issue. As I said previously, for Blue Pill boards, most probably they contain a counterfeit chip.

 


@dv4 wrote:
 I am using an ST-Link V2

This one? (a post from @Andrew Neil from this knowledge base article:(

mALLEm_1-1771491103620.png

If yes, that could be also another problem.

So please use one of the ST boards that contains a genuine chip and STLINK.

You can purshase: the nucleo board: NUCLEO-F103RB

It contains a STM32F103 genuine chip as well as a genuine ST-LINK:

mALLEm_2-1771491269868.png

Hope that helps.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."