Skip to main content
SJ.8
Visitor II
April 8, 2022
Question

Hi, I need TJ(Junction Temperature) and RJA( Junction to ambient Thermal resistance) of M24C02-RMN6TP EEPROM for Derating. Can you provide. Regards, Srinivas

  • April 8, 2022
  • 1 reply
  • 1148 views
This topic has been closed for replies.

1 reply

Peter BENSCH
Technical Moderator
April 8, 2022

This EEPROM has a maximum current consumption of 1mA at 5.5V. We are therefore talking about a maximum power loss of 1mA*5.5V=5.5mW.

Even if we assume a completely unrealistic value of 100K/W for Rja, this would result in a temperature increase of 0.55K. In this respect, the ambient temperature can be regarded as identical to the junction temperature. Calculating a derating on this basis is therefore meaningless.

Does it answer your question?

Regards

/Peter