the data sheet of the STWBC2-HP already contains two example circuits with single coil, see there page 4 and page 5.
Otherwise you will also find an example with multi-coil in the reference design STDES-50W2CWBC. There, two coils are controlled, but this can easily be reduced to one coil by leaving out one branch, i.e. e.g. the lower Qi coil, C410, C412, C415, Q408, Q409.
1/ In this eval board https://www.st.com/en/evaluation-tools/stdes-50w2cwbc.html you used variable frequency full-bridge configuration, right? -What changes are required if I want to use fixed frequency configuration? A:Yes Full bridge, if you want to use fixed frequency, it need speical FW to support this.
2/ If I want to use STWBC2-HP with qi1.3, I need to add Stsafe and NFC? Is there others requirements? A: Yes, you need add STSAFE and update to lastest FW.
3/ What is the efficiency of STWBC2-HP? A: It depend on RX and coil and system efficiency is about 85%.
For more information please refer to STWBC2-HP - Qi-compatible inductive wireless charger power transmitter for up to 100W applications - STMicroelectronics Please give your company email for future support.
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.