Skip to main content
PGrad.1
Associate II
April 26, 2022
Solved

HI, we have 74V1T07STR, with marking "TL", but datasheet not labeled. How can I make sure that the IC - 74V1T07STR ?

  • April 26, 2022
  • 2 replies
  • 1598 views

I have a photo with a label

This topic has been closed for replies.
Best answer by Peter BENSCH

The component has been discontinued for many years, unfortunately there is no documentation left.

I'm afraid the only chance to find out is an electrical test circuit of the logic function. The 74V1T07 was a simple logic buffer with:

  • pin2 = input
  • pin4 = output
  • pin3 = GND and
  • pin5 = VCC (4.5...5.5V, max ICC=1µA)

If you apply TTL signals, you get the same signals from the output.

Does it answer your question?

Good luck and regards

/Peter

2 replies

PGrad.1
PGrad.1Author
Associate II
April 29, 2022

...

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
April 29, 2022

The component has been discontinued for many years, unfortunately there is no documentation left.

I'm afraid the only chance to find out is an electrical test circuit of the logic function. The 74V1T07 was a simple logic buffer with:

  • pin2 = input
  • pin4 = output
  • pin3 = GND and
  • pin5 = VCC (4.5...5.5V, max ICC=1µA)

If you apply TTL signals, you get the same signals from the output.

Does it answer your question?

Good luck and regards

/Peter

PGrad.1
PGrad.1Author
Associate II
April 29, 2022

Thank you, Peter Bensch!

I will do that, thanks for the tip

Have a nice day

/PGrad.1