Skip to main content
Visitor II
May 27, 2025
Solved

High optimization of IAR Embedded Workbench 9.60.3

  • May 27, 2025
  • 1 reply
  • 410 views

What does the 'High' optimization  actually do in IAR Embedded Workbench 9.60.3 when the 'Size' option is selected, but no additional optimization checkboxes are enabled. Even without selecting any extra options(like CSE, loop unrolling, etc. ), the code size reduces significantly—up to 30%. How is the  IAR Embedded Workbench 9.60.3 achieving this reduction, and what specific optimizations are being performed in this case.

Best answer by Peter BENSCH

Welcome @Abdul_Aziz, to the community!

the IAR Embedded Workbench is a product of IAR, so this question can probably only be answered by someone from IAR, if they happen to be reading here.

But it would probably be better if you asked the support of IAR?

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
May 27, 2025

Welcome @Abdul_Aziz, to the community!

the IAR Embedded Workbench is a product of IAR, so this question can probably only be answered by someone from IAR, if they happen to be reading here.

But it would probably be better if you asked the support of IAR?

Regards
/Peter