Skip to main content
RThom.9
Visitor II
November 24, 2022
Solved

I am looking for the reverse characteristics of STTH2R02AF-Y. How much will be the leakage power at 60V and 48V. Where should I get the Leakage current graphs wrt reverse voltage (not in datasheet)

  • November 24, 2022
  • 1 reply
  • 872 views

..

This topic has been closed for replies.
Best answer by GJEAN.1

Hello @Community member​ ,

Indeed, leakage current (IR) curves are not given in STTH2R02AF-Y datasheet, because the values are quite very low => negligible in power applications.

However, in table 4 IR values at 200V, 25°C and 125°C are given (typical and maximum values: 1µA/8µA).

0693W00000WKlpiQAD.png 

The maximum leakage current you get at 200V 125°C is 8µA. For a constant reverse voltage of 200V, Prev = 800V*8µA = 1.6 mW.

At 60V the values will be lower by decade at least => so totally negligible.

Best regards

1 reply

GJEAN.1
GJEAN.1Best answer
Visitor II
December 12, 2022

Hello @Community member​ ,

Indeed, leakage current (IR) curves are not given in STTH2R02AF-Y datasheet, because the values are quite very low => negligible in power applications.

However, in table 4 IR values at 200V, 25°C and 125°C are given (typical and maximum values: 1µA/8µA).

0693W00000WKlpiQAD.png 

The maximum leakage current you get at 200V 125°C is 8µA. For a constant reverse voltage of 200V, Prev = 800V*8µA = 1.6 mW.

At 60V the values will be lower by decade at least => so totally negligible.

Best regards